Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
codewarrior-slide5

Selecting the right suite to fit the customer’s needs is easy. The first step is to determine whether the perpetual or annual subscription option is the best fit. Second, determine the level of suite based on the project requirements. Focus on the tools the designer wants and pick the suite level that contains it. Finally, determine the licensing model. If the customer would like to tie the license to one computer or a USB license dongle, select Node-Locked, or if wanting to tie the license to a server and access it via the network, select a Floating license. Additionally, after the first year of technical support expires, it is easy to renew.

PTM Veröffentlicht am: