Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Product List
Model 3255A DC Accelerometer Slide 2

TE Connectivity is a global designer and manufacturer of sensors and sensor-based systems which measure pressure/force, position, vibration, temperature, humidity, and fluid properties. The products are used as embedded devices by original equipment manufacturers (OEMs) or as stand alone sensors for test and measurement to provide critical monitoring, feedback and control input. They are at the heart of many everyday products and provide a vital link to the physical world. The model 3255A is a miniature, DC accelerometer featuring silicon MEMS technology. It has low DC power requirements, amplified voltage output and utilizes ceramic construction for ease of solder mounting. Offered in low to high g ranges, this device is hermetically sealed and gas damped. All units have a DC response and are shipped with an NIST traceable statement of calibration. A one year replacement warranty is provided.

PTM Veröffentlicht am: