Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Metal Oxide Varistor (MOV)

To understand how an SPD works, the customer needs to look at MOVs. MOVs are typically made of zinc oxide and are connected in parallel. MOVs are bi-directional and will begin conducting when a threshold voltage is achieved. When below the voltage, resistance is high and a trivial amount of current will flow through the MOV. Once the threshold voltage is met (typically 115% rated voltage), the resistance drops very low to almost 0 ohms and voltage will flow through the MOV as current, rather than the load. When the voltage drops below the threshold, the MOV resistance increases and stops clamping the overvoltage.

PTM Veröffentlicht am: