Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
APD-Slide9

In this example, note that the filter capacitors have been removed from across the photodiode and on the feedback node in order to obtain a fast transient response. The LT1815 is simply used to measure the transient. The timing scope photo shows that the response time is well within the 100ns limit. For a more complete write-up on APD transient measurement techniques, see LTC Design Note 447.

PTM Veröffentlicht am: