Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
LTC4310-Slide2

The LTC4310 is a hot swappable I²C isolator that provides fully bidirectional communication between two I²C busses whose grounds are isolated from one another. Clock stretching, clock synchronization, and arbitration work seamlessly across the isolation barrier. I²C isolation has traditionally been achieved using up to four optocouplers and special buffers; a costly, large, and relatively complicated technique. Using the LTC4310 simplifies I²C isolation by encoding and transmitting I²C bus signals over an isolation barrier. The signals are decoded and recombined on the other side of the barrier using a second LTC4310 all while maintaining I²C signal integrity. The LTC4310 allows the signals to be bridged by an Ethernet transformer to achieve communications across voltage differences of more than 1500VRMS, or capacitors can be used for lower voltage differentials. The LTC4310-1 is intended for use in 100kHz standard mode I²C systems while the LTC4310-2 is designed for 400kHz fast mode I²C systems. Compliant logic low thresholds on both sides of the LTC4310 ensure compatibility with other I²C devices while also providing generous noise margins for heavily capacitive busses.

PTM Veröffentlicht am: