Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Image of KEMET Comparing Tantalum Polymer and MnO2 Capacitors - Cathode

The important properties required for the primary cathode material in a solid electrolytic capacitor is the ability to impregnate small pores, high conductivity, low cost, and the most restrictive requirement is the ability to form a non-conductive plug to ‘heal’ leakage sites in the dielectric. Joule heating at a leakage site converts the primary cathode material to a non-conductive material. For example, the MnO2 is converted to Mn2O3 at a temperature of about 500°C. Conductivity is another critical property of the primary cathode material. The difference of conductivity between the conductive polymers and the MnO2 was the primary reason for introducing this material in tantalum capacitors as a method to obtain lower ESRs.

PTM Veröffentlicht am: