Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
order info
The KPS-MCC series part number can be constructed using the ordering code shown here. To construct the KEMET part number, refer to the waterfall table in the KPS-MCC datasheet. Locate the section of the waterfall table that corresponds to the required rated voltage. Find the capacitance value that is required and record the base part number. The lead configuration can be selected using the fourth character position. Character positions 11 and 12 can be used to select the capacitor tolerance and lead termination finish.
PTM Veröffentlicht am: