Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
driver stage with double fold back

OVP transceivers with wide common-mode ranges require double fold-back current limiting within the driver stage. The above diagram shows the current limiting function of the ISL3245xE family of OVP transceivers that operate over a ±20 V common-mode range. Here the first fold-back current level of 63 mA ensures that the driver never folds back when driving loads within the 40 V common-mode range. The very low second fold-back current setting of 13 mA minimizes power dissipation if the driver is enabled when a fault occurs. This current limiting scheme ensures that the output current never exceeds the RS-485 specification, even at the extremes of the common-mode and fault condition voltage range.

PTM Veröffentlicht am: