Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
wizard all Power Module Wizard login
When clicking on the “Stability Analysis” button, a full page bode plot will appear for review and documenting. When clicking on the "Load Transient" button, a full page graph showing the actual voltage response to a load transient will appear. These graphs also have markers if the user would like to make specific measurements of the plots. Additionally, a user can also view a graph of the module's specific efficiency curve as well as input and output ripple noise characteristics. It is important to note all this analysis is calculated in real time, affected by how the module is being used and the external components attached to it. So if there are changes to the external components, filtering, trim resistor (for output voltage programming), or the RTUNE/CTUNE components, there will be notable differences in the output of all of the analysis selections.
PTM Veröffentlicht am: