Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
summary
In summary, NXP’s long-standing history as an innovative leader has led its expanding product families down the same pioneering path. From low noise amplifiers to air cavity and over molded packaging, NXP RF has always been setting standards in the radio frequency market. These characteristics are also shown through the offerings in NXP’s amplifier portfolio. This MMIC product line contains devices that offer up to 850 mA supply current, operate across a wide range of frequencies (between DC and 6000MHz), and can achieve very low noise parameters.
PTM Veröffentlicht am: