Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Image of EDAC Card Edge Connectors - Polarization

A polarizing key is a feature that can be added to a card edge connector so that only the proper PC board can be inserted into the connector. The key acts as a stop and prevents improper boards from being inserted into the connector. Only boards with a cut out matching the location of the polarizing key in the connector can be inserted into the connector. The key also prevents a PC board from being inserted incorrectly/backwards into the connector.

PTM Veröffentlicht am: