Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
High Power LED Driving Solutions - ZXLD1350 Slide 13

To summarize, C1 is a 1 µF ceramic at a voltage rating 10% greater than VIN Max. This must be an X7R not aY5V ADJ can be left floating but if the user wants to increase noise immunity on the pin add a 10 nF ceramic capacitor. C3 reduces ripple current in the LED. Without it the LED is subject to peak currents of +/-15% of the average current. Adding a 1 µF X7R rated at the VIN voltage will reduce this to under about a factor of 3. This has no effect on efficiency or frequency but does increase start up delay.

PTM Veröffentlicht am: