Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Wi-Fi-Cloud-Slide9

The user will then connect to the default dashboard, which includes a variety of fully customizable widgets. Using these widgets, the user can interact with the development board from anywhere in the world with an internet connection – turn on switches, LEDs, vibration motor, view readings from sensors on the development board, or build ones own custom internet-connected sensor and an associated widget to monitor or control it. 

PTM Veröffentlicht am: