Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Mapping a Digi XBee IoT Network with Digi XCTU Slide 9

For Digi XBee models prior to the Digi XBee3, developers can create end devices by loading the Zigbee End Device AT firmware and resetting the module. This will automatically enable cyclic sleep mode. Remember that end devices will only talk to their “parent” radio module, a relationship negotiated when the module starts up. They are not directly part of the mesh so users will only see one connection to the current parent on the map. Designers will be ready to go once they have the following set up:  One Digi XBee configured as a Zigbee coordinator.  One Digi XBee (Zigbee coordinator or router mode) connected to their computer and configured for API mode, and all the remaining Digi XBees configured as either Zigbee routers or end devices, and powered on.

PTM Veröffentlicht am: