Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
DIP-Switch-Slide5

The next three slides will describe the different switching methods that are available. Shown in the top view is the single pole single throw, which is one individual switch that is opened and closed with the movement of the actuator. The double pole single throw switch shown below, is two sets of contacts (or two switches) that are opened and closed simultaneously with the movement of a single actuator.

PTM Veröffentlicht am: