Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
ADF7xxx ISM Transceivers Slide 10

The ADF7021 takes the performance beyond that of the ADF7020 with Rx sensitivity increased to -123dBm at 1kbps or -130dBm at 100bps. The ADF7021 has improved AFC performance and the power amplifier or PA meets the new ETSI specification for avoiding transient spurs when turning on/off. The device also supports FCC Part 90 in the USA, ETSI EN300-220 in Europe, ARIB STD-T67 in Japan as well as the Chinese & Korean Standards.

PTM Veröffentlicht am: