Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
RMS-DC-Slide7

Dynamic range is the span between the largest and smallest input signals. The wider the dynamic range of RMS-to-DC converters, the simpler the system designs can be. This makes larger signals and low level error voltages easier to process. As shown here, the AD8436 has the ability to directly process signals as low as 100µVolts RMS.

PTM Veröffentlicht am: