Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Surveillance-Slide5

Some customers may want to keep their existing back-end encoding solution (e.g. an ASSP or DSP-based H.264 encoder). Intel® offers a smaller FPGA providing only the required elements of the pipeline that can enable the entry of WDR CMOS sensors in surveillance cameras. In this case, the front-end blocks from Apical (acquired by Arm®) remain, but the back-end removes the H.264 encoding and Ethernet MAC. It is replaced by a standard RAW or BT.1120 output that can connect to today’s typical ASSP or DSP-based encoder ICs.

PTM Veröffentlicht am: