Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
A495x-Slide17

Initially the output turns on and current in the load increases until it reaches the peak current limit as set by the sense resistor and the voltage on the VREF pin. Once the peak current is reached the device automatically initiates its internal crossover current protection which prevents shoot-through in the bridge and starts the fixed off time timer.

PTM Veröffentlicht am: