Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
CFast-Slide8

The 3M ejector for the CFast card connector is modeled after the design for the CompactFlash card connector. The ejector unit snaps securely over the connector. A pivoted lever attaches to a slider which offers the user a dual push button for gently releasing the card. The ejector is sold separately, however the connector is also available with the ejector attached and ready to use out of the box.

PTM Veröffentlicht am: