Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
UHM- Slide9
Compared to an unshielded 2mm HM connector the fully shielded UHM connector displays significantly reduced crosstalk. In addition, the UHM shield design provides a controlled impedance path which minimizes insertion loss and rise time degradation. A key point is that by improving the signal isolation, more of the signal pins can now be used for high speed signals significantly increasing the number of channels available for transmission compared to the unshielded 2mm HM connector pin-outs – as a matter of fact, as many as two times more channels can be used for high speed signals.
PTM Veröffentlicht am: