Maker.io main logo

Using macros and snippets with Keybow

25

2023-05-25 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

The real power of Keybow and Keybow MINI is in its ability to become a ‎macro keyboard, triggering a whole series of keypresses from just a single ‎key, for example "control-alt-delete" or typing "The quick brown fox jumps ‎over the lazy dog". This is great for setting up actions that you can never ‎quite remember, like the shortcut to import photos to Lightroom ‎‎(command/control-shift-I), by just linking them to a single key.‎

You could also create a Keybow layout that stored all your frequently used ‎bits of text, like code snippets, email templates, or even complex sets of ‎actions like opening a web browser, then entering an URL or search term and ‎hitting enter. The world is your lobster!‎

As well as these custom actions, we've put together a couple of files full of ‎handy snippets for Windows and Mac; these are common actions like ‎peeking the desktop, snapping windows to one side or the other, a Spotlight ‎search on Mac, and lots more. You can link these straight to keypresses in ‎your layout files.‎

We'll assume that you've followed the first two Keybow tutorials already, but ‎if you haven't then go back over them before this one:‎

If you have a Keybow MINI and need to assemble it, then follow this ‎tutorial: Assembling Keybow MINI

Note that if you're using Keybow MINI then you'll need to add the following ‎bit of code just after the require "keybow" in your layout ‎file, and substitute handle_key_00 for handle_minikey_00 in each of your key ‎mapping functions.‎

Creating a simple macro

We'll create a simple Windows-R (opens the run menu on Windows; if you're ‎on Mac then these keys will refresh your browser page) macro as an ‎example of how to put them together, and how to use modifier keys and the ‎tap key function.‎

Unplug the USB cable from your Keybow or Keybow MINI and pop the micro-‎SD card out and put it in your computer. In the layouts folder, create a new ‎layout called macros.lua and add the following to it:

Copy Code
require "keybow"

function handle_key_00(pressed)
if pressed then
keybow.set_modifier(keybow.LEFT_META, keybow.KEY_DOWN)
keybow.tap_key("r", pressed)
keybow.set_modifier(keybow.LEFT_META, keybow.KEY_UP)
end
end

Let's break down what the code does.

‎The macro is bound to key 0, that is the bottom left key when Keybow is in ‎portrait orientation with the USB cable at the right-hand side.‎

We're running this macro when the key is pressed (as opposed to when it's ‎released), hence the if pressed then.‎

The line keybow.set_modifier(keybow.LEFT_META, keybow.KEY_DOWN) uses ‎the set_modifier function that allows you to keep a modifier key held down while ‎you press another key or keys and tells Keybow to keep the key held down -‎‎ keybow.KEY_DOWN. keybow.LEFT_META represents the Windows key on Windows or ‎the command key on Mac.‎

Next, we use the tap_key function, which simulates a quick press and release ‎of a key, to tap the "r" key - keybow.tap_key("r", pressed).‎

Last of all, we use the set_modifier function again to release ‎the keybow.LEFT_META (Windows) key - keybow.set_modifier(keybow.LEFT_META, ‎keybow.KEY_UP), before closing both the if statement and the handle_key function ‎with end.‎

Save your new macros.lua file in the layouts folder, and then open the keys.lua file ‎and link and enable your new layout. The file should look something like this:‎‎

Copy Code
```lua
require "keybow"

-- require "layouts/default" -- Numberpad

-- Custom layouts (uncomment to enable) --

-- require "layouts/boilerplate" -- Handy bits of boilerplate text like Lorem Ipsum
-- require "layouts/lightroom" -- Handy hotkeys for Adobe Lightroom Classic CC
-- require "layouts/pico8" -- Controls for Pico-8

require "layouts/macros" -- Macros layout

Save the keys.lua filem, eject and pop the micro-SD card out and into your ‎Keybow, then plug it in with its USB cable. Once booted, give your new macro ‎a try!‎

Entering strings of text

Entering strings of text can be really handy. It might be a snippet of text that ‎you use frequently, like an address or some Lorem Ipsum placeholder text, or ‎it could be a search term that gets entered once you've opened your web ‎browser with a macro.‎

Here, we'll extend our Windows-R run menu macro that we made and type ‎‎"cmd" to open the command prompt, and then tap enter to open it. We'll also ‎use the keybow.sleep() function to introduce a couple of short pauses between ‎the parts of the macro.‎

Disconnect your Keybow or Keybow MINI, remove the micro-SD card again, ‎and pop it into your computer. Open the macros.lua file.

‎Within the handle_key_00 function that we added our macro to, add ‎a keybow.sleep(500) straight after the keybow.set_modifier(keybow.LEFT_META, ‎keybow.KEY_UP) line. This will introduce a half-second (500 milliseconds) pause ‎before the next line in our macro.‎

Next, we'll use the keybow.text() function to type our "cmd" text. Add the ‎line keybow.text("cmd") below the keybow.sleep(500) line.‎

You can use the keybow.text() function with any of the text characters on your ‎keyboard, including shifted characters (uppercase letters, !, @, £, etc.), and ‎also spaces, and even tabs and new lines with \t and \n respectively.‎

Add another keybow.sleep(500) below that last line to introduce another small ‎pause.‎

Last of all, we'll add the line keybow.tap_enter() to tap the enter key. There ‎are keybow.tap_ functions for several of the most commonly used keys like ‎enter, space, and tab, as well as the tap_key() function that we used earlier, to ‎which you can pass any key to tap it. You can see them all towards the ‎bottom of the keybow.lua file.‎

Your whole macros.lua file should now look like this:

Copy Code
require "keybow"

function handle_key_00(pressed)
if pressed then
keybow.set_modifier(keybow.LEFT_META, keybow.KEY_DOWN)
keybow.tap_key("r", pressed)
keybow.set_modifier(keybow.LEFT_META, keybow.KEY_UP)
keybow.sleep(500)
keybow.text("cmd")
keybow.sleep(500)
keybow.tap_enter()
end
end

Save that file, eject the micro-SD card, and pop it into your Keybow. Does the ‎macro work, and open the command prompt?

‎If you're using a Mac, then you can change this macro example to hold ‎command, tap space, and then type something like "chrome" to open Google ‎Chrome.‎

Using the ready-made snippets for Windows and Mac

We've included a folder called snippets with two files ‎in, windows_snippets and mac_snippets. These files have a whole bunch of ‎readymade functions - hotkeys and macros - that you can use directly in your ‎layouts. They cover basic things like switching between app windows, ‎snapping windows, opening spotlight, or Windows search, and a lot more.‎

We'll put together an example that uses a couple of the Mac snippets to do ‎something that you probably do several times a day, but now you can do it ‎with just a single keypress - search for cat GIFs!‎

Let's add this new macro to our 'macros.lua' file that we've been using and ‎assign it to key 1 (the middle bottom key). Think about the steps involved in ‎doing our cat gifs search. We have to:

  1. ‎‎Open Spotlight‎
  2. Get Spotlight to open Safari‎
  3. Focus on the smart search field
  4. Type in "cat gifs" and press enter

Luckily, there are snippets we can use to do the trickier steps of a Spotlight ‎search and the Safari search, so it's just a case of adding two lines rather ‎than a whole bunch.‎

Disconnect your Keybow or Keybow MINI, remove the micro-SD card, and ‎pop it into your computer. Open the macros.lua file.

‎At the top of the file, just below the require "keybow" line, add require ‎‎"snippets/mac_snippets". This will let us use functions from the mac_snippets.lua file in ‎the snippets folder.‎

Create a new handle_key function at the bottom of your macros file, which ‎looks like this:‎

Copy Code
function handle_key_01(pressed)
if pressed then
mac_snippets.spotlight("safari")
mac_snippets.safari_search("cat gifs")
end
end

Remarkably easy, huh? The spotlight and safari_search snippets take a string as ‎input and handle the other parts of the process, i.e., the keyboard shortcut, ‎entering the text, and then pressing enter.‎

Your whole macros.lua file should now look like this:‎

Copy Code
require "keybow"
require "snippets/mac_snippets"

function handle_key_00(pressed)
if pressed then
keybow.set_modifier(keybow.LEFT_META, keybow.KEY_DOWN)
keybow.tap_key("r", pressed)
keybow.set_modifier(keybow.LEFT_META, keybow.KEY_UP)
keybow.sleep(500)
keybow.text("cmd")
keybow.sleep(500)
keybow.tap_enter()
end
end

function handle_key_01(pressed)
if pressed then
mac_snippets.spotlight("safari")
mac_snippets.safari_search("cat gifs")
end
end

Eject the micro-SD card, put it into your Keybow or Keybow MINI, then plug it ‎into your computer. Press key 1 and... SHAZAM... cat GIFs!‎

Take a look though the windows_snippets and mac_snippets files in the snippets folder ‎to see all of the functionality included everything from general navigation ‎shortcuts to screenshots, to specific app shortcuts for Safari, Chrome, and ‎email.‎

That's all folks! ‎ ‎

Herst.-Teilenr. PIM451
KEYBOW MINI MACRO PAD KIT - LINE
Pimoroni Ltd
Herst.-Teilenr. PIM565
SWITCH KEYPAD 16KEY CLICKY
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.