Maker.io main logo

Control a CC3200 LaunchPad with your phone using Blynk

62

2016-02-18 | By daniel_ohh

License: Attribution Launchpad

The goal of this project is to get a CC3200 connected to a Blynk app on either your Android or iOS device. Blynk is an IoT platform that lets you create a custom mobile app to communicate with an internet connected microcontroller.

The Texas Instruments CC3200 LaunchPad is a great candidate for this project. It's powerful Wi-Fi SoC allows us to easily connect to the internet and the on-board BMA222 Accelerometer and TMP006 infrared temperature sensor will let us read some useful data without any external components.

The Blynk App

First, let's create the mobile application. To start, create a Blynk account by installing the Blynk app on your Android or iOS device. In the app, click the button to create a new project. Name your project, and select TI-CC3200-LaunchXL for your hardware. You will also see an Auth Token created for you. This is specific to your project and how the Blynk App will identify the CC3200 LaunchPad.  Go ahead and email this token to yourself so you can copy and paste it into your app later. 

Blynk new project

Next, add the necessary widgets to your app with the button. Add 3 Graph widgets, 1 Button widget, and 1 Value Display widget.  Configure them as show in the screenshots below.

 Blynk - add buttons
The Red LED is assigned to Virtual Pin 1, and the temp sensor is assigned to virtual pin 5. The app will send button press information to the launchpad and request temperature readings once per second.
 
Blynk graph settings
The X, Y, and Z axes of the accelerometer are assigned to virtual pins 7, 8 and 9. The app will request their values from the LaunchPad every 250ms.
 

Each of the widgets is assigned a virtual pin. We will use these virtual pins in the embedded code to communicate with the app. You will see in the code below where we define the button (V1) to control the Red LED on the LaunchPad, V5 to read the temperature sensor, and V6-V8 to read the accelerometer data.  

I arranged the widgets in my app like this:

Blynk widget layout

The Embedded Code

If you haven't, install Energia.  You can find download links and some more information about Energia here: www.energia.nu 

Now, download the Blynk libraries here: https://github.com/blynkkk/blynk-library/releases 

Extract the .zip file and copy the folder "Blynk" and "SimpleTimer" to \energia-0101E0017\hardware\cc3200\libraries\ (this may vary depending on where you installed Energia.)

Launch Energia and create a new project. Copy the code below, add in your authorization token (from the Blynk app) and your WiFi credentials. Make sure you have CC3200LP selected in Tools > Board and the correct port selected in Tools > Serial Port.  

Press the "play" button in the Blynk app to deploy your app.

In the serial terminal, you should see the LaunchPad connect to your WiFi network and display the temperature each time the app requests data from the board.

Demo

Demo

The Code

Make sure you update with your Auth Token and WiFi credentials.

Copy Code
/**************************************************************
* Blynk is a platform with iOS and Android apps to control
* Arduino, Raspberry Pi and the likes over the Internet.
* You can easily build graphic interfaces for all your
* projects by simply dragging and dropping widgets.
*
* Downloads, docs, tutorials: http://www.blynk.cc
* Blynk community: http://community.blynk.cc
* Social networks: http://www.fb.com/blynkapp
* http://twitter.com/blynk_app
*
* Blynk library is licensed under MIT license
* This example code is in public domain.
*
**************************************************************
* This example shows how to use TI CC3200-LaunchXL
* to connect your project to Blynk.
*
* Feel free to apply it to any other example. It's simple!
*
**************************************************************/

#define BLYNK_PRINT Serial // Comment this out to disable prints and save space
#include <SPI.h>
#include <WiFi.h>
#include <BlynkSimpleTI_CC3200_LaunchXL.h>
#include <Wire.h>
#include "Adafruit_TMP006.h"
#include <BMA222.h>

// Sensor objects
BMA222 mySensor;
Adafruit_TMP006 tmp006(0x41);

// You should get Auth Token in the Blynk App.
// Go to the Project Settings (nut icon).
char auth[] = "XXXXXXXXXXXXXXXXXXXXXXXXXX";

// Your WiFi credentials
char ssid[] = "YOUR SSID HERE";
char pass[] = "YOUR WIFI PASSWORD HERE"; // Set to "" for open networks
int dataX = 0;
int dataY = 0;
int dataZ = 0;

void setup()
{
//Open a serial terminal with the PC
Serial.begin(9600);
//Set up a blynk connection with your WiFi credentials
Blynk.begin(auth, ssid, pass);

//Accel. setup
mySensor.begin();

//TMP006 setup
tmp006.begin();

//Setup RED LED to be an output
pinMode(RED_LED, OUTPUT);
digitalWrite(RED_LED, LOW);
}

// Virtual Pin 1 - Toggles the LED high or low depending on the mobile app input
BLYNK_WRITE(V1)
{
//Print to the terminal
BLYNK_LOG("Got a value: %s", param.asStr());

//save teh value fromt he app to the variable i
//if i=1, turn the LED on
//if i=0, turn the LED off
int i = param.asInt();
if(i == 1)
{
digitalWrite(RED_LED, HIGH);
}
else if(i == 0)
{
digitalWrite(RED_LED, LOW);
}
}

//Virtual pin 5 - Read the TMP006 value when called by the app
BLYNK_READ(5)
{
float objt = tmp006.readObjTempC();
Serial.print("Object Temperature: ");
Serial.print(objt);
Serial.println("*C");
Blynk.virtualWrite(V5, (int)objt);
}

// Virtual Pin 6
// When virtual pin 6 is requested by the mobile app, we
// will also send data for pins 7 and 8 so all 3 graphs
// are updated
BLYNK_READ(6)
{
//Send X axis data
dataX = mySensor.readXData();
Blynk.virtualWrite(V6,dataX);
//Send Y axis data
dataY = mySensor.readYData();
Blynk.virtualWrite(V7,dataY);
//Send Z axis data
dataZ = mySensor.readZData();
Blynk.virtualWrite(V8,dataZ);
}

// The main loop listens for commands from the mobile app
void loop()
{
Blynk.run();
}
Herst.-Teilenr. CC3200-LAUNCHXL
LAUNCHPAD DEV BOARD CC3200
Texas Instruments
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.