Maker.io main logo

Programmable 12v Outdoor Cafe Lights

36

2024-07-30 | By Adafruit Industries

License: See Original Project LEDs / Discrete / Modules

Courtesy of Adafruit

Guide by Erin St Blaine

Overview

 

Cafe-style light strands with Edison bulbs are a beautiful way to ‎decorate your patio. They are a fantastic and classy way to light up ‎any outdoor space. Wineries, bistros, and night markets use them to ‎create a cozy, intimately lit space that's warm and inviting to diners, ‎and they look fabulous in backyards of just about any size.‎

These lights are a programmable, addressable version of the cafe ‎market lights you can find at the hardware store. Add Arduino or ‎CircuitPython code and you can turn your lights on in party mode, ‎sending warm rainbow animations across your yard. ‎

These lights require 12v power, and also need to hold up in an ‎outdoor environment. This guide will focus on how to power a 5v ‎microcontroller and 12v lights from the same setup, and also show ‎how to use a waterproof enclosure to keep your lights safe from rain ‎and weather.‎

lights_1

These are 12v lights with 50cm spacing between them. Each strand ‎has 30 bulbs and they come with waterproof connectors on each ‎end.‎

I got them from Ray Wu's store on AliExpress, which had the best ‎deal I could find for this kind of light. They are available in different ‎spacings and different voltages - be sure you get the 12v kind and ‎not the 24v for the scope of this guide.‎

I plugged 4 strands into a daisy-chain, for a total of 120 lights, ‎without a noticeable voltage drop. ‎

stringlights_2

Additional Parts Needed

These lights require 12v power, but our microcontrollers need 5v ‎power. This DC Power BFF is what we need. It can receive and ‎deliver 12v power through its screw terminal port and 2.1mm jack, ‎and at the same time, deliver 5v power to the microcontroller ‎through the headers. ‎

Since this is an outdoor installation, it's a good idea to place the ‎electronics inside a weatherproof box to protect them from the ‎elements. This box is just the right size and has two cable glands for ‎passing power and data wires. ‎

Power Supply

These lights require a 12v power supply. We have a few in the ‎shop which are great for indoor installations, but if you're putting ‎these out in the garden it's a good idea to look for an outdoor 12v ‎power supply.‎

Here's the one I ended up using. It's made for landscape lighting, so ‎it's completely weather-proof, and it has some cool additional ‎features like a built-in timer and an automatic light sensor that turns ‎your lights on at sunset. ‎

  • ‎60W Outdoor 12v Power Supply‎

This one is rated for 60W, which is way more than I need for this ‎strand of lights, but since I am planning on adding additional ‎landscape lighting to my yard, I went with a solution that will allow ‎for some expansion.‎

power_3

Depending on your power supply and setup, you may find it handy ‎to pick up a couple of screw terminals. This male one fits into the ‎Power BFF.‎

Tools & Additional Materials

  • Soldering iron & accessories
  • Heat shrink tubing
  • Small & standard sized screwdrivers
  • Light socket plug adapter, in case you don't have a power outlet ‎handy

Wiring Diagram

topower_4

The power BFF stacks on top of the QT Py using the included female ‎headers.‎

The data pin from the LEDs is connected to the yellow stemma wire ‎‎(SCL) and plugs into the QT Py via the Stemma port.‎

The LED strand and the power supply's power and ground wires ‎both get connected to the Power BFF.‎

In this diagram the LEDs are wired into the screw terminals and the ‎power supply is plugged into the 2.1mm jack. As long as both are ‎connected, these two ports are interchangeable, so use whichever ‎makes sense with your power supply.‎

Software

The QT Py is compatible with Arduino and with CircuitPython, so you ‎have plenty of options when it comes to coding your lights. ‎

Here are some guides with sample code that can get you started. ‎You may need to make a few changes to the code samples, but ‎these projects can fairly easily be modified to work on the QT Py.‎

Or head to the next page for a step-by-step guide to installing a ‎beautiful animation using Arduino.‎

Arduino Code

This code example uses the FastLED library and is modified from a ‎sketch called DesignerPalettes by Mark Kriegsman.‎

It's a great idea to get your software all set up and loaded onto your ‎board right away, to make testing your connections easier later on.‎

To get the code running you'll need:‎

  1. Arduino IDE (1.8 or newer)‎‎
  2. Adafruit Board support for QT Py‎
  3. Arduino libraries: FastLED, Adafruit_NeoPixel

‎1. Arduino IDE‎

If you’re not using a recent version of the Arduino IDE, this would be ‎a good time to upgrade. If this is your first time using Arduino, head ‎over to this guide to get it installed. It's free and fairly simple to get ‎set up.‎

‎2. Board Support‎

You'll need to tell the Arduino IDE which board you're using. This ‎takes just a few minutes of setup, and you'll only need to do it once. ‎

Here is a step-by-step tutorial for setting up QT Py

‎3. Libraries‎

Both libraries can be installed using the Arduino Library Manager — ‎use Sketch → Include Library → Manage Libraries… and search for all ‎or part of the library’s name, then click “Install.”‎

Look for:‎

  • FastLED
  • Adafruit_NeoPixel

Adafruit_NeoPixel isn’t absolutely required for this project, but it’s ‎handy to have installed in case you have problems with FastLED. ‎Troubleshooting the basics is a little easier with Adafruit_NeoPixel.

Upload the Code

Get the code by clicking "Download Project Zip" in the code listing ‎below. Unzip the code into your Arduino project folder.‎

Plug your microcontroller into your computer with a USB cable. In ‎the Arduino IDE, go to File -> Open to open the code file. Go to Tools ‎‎-> Boards and select the name of the board: Adafruit QT PY ‎‎(SAMD21). Then go to Tools -> Port and select the board there ‎too. (If it's not showing up there, be sure your microcontroller is ‎plugged into your computer via USB.)‎

Download File

Copy Code
Temporarily unable to load content:

View on GitHub

Creating Color Palettes

 

FastLED Color Palettes

Using the FastLED library opens up a world of LED coding tools that ‎are fairly easy to use. ‎

There's a fantastic tool called PaletteKnife that works great for artist-‎minded people who think in colors instead of in code, and this ‎project uses it. ‎

Watch the video above for a demo of just how easy this is.‎

Want to try PaletteKnife and grab some new color palettes?

Here's what you'll definitely need:‎

  1. A basic understanding of how FastLED palettes are ‎used. Check out the FastLED ColorPalette example, as well as ‎FastLED Fire2012WithPalette example, both of which can be ‎found in the FastLED library Examples folder.‎‎
  2. You'll need Chrome or Safari. PaletteKnife doesn't work with ‎Firefox or IE.‎‎
  3. You will also need a little patience; it's not terribly slick but it ‎works a dream.‎

Basically, you browse to the color palette that you want, and click ‎PaletteKnife (a bookmarklet) in your browser. Then you COPY the ‎resulting code and PASTE it into your FastLED animation source ‎code. ‎‎

Full instructions on how to get started with PaletteKnife are here:‎‎ http://fastled.io/tools/paletteknife/‎

palette_4a

assembly_5

Electronics Assembly

Solder the headers to the top / front of the QT Py. The easiest way to ‎do this is to place the headers into a solderless breadboard with the ‎short ends up, and set the QT Py on top upside-down, so you're ‎soldering to the back of the board.‎

solder_6

The QT Py will plug in to the female headers on bottom of the BFF. ‎Be sure the USB port on the QT Py is aligned with the 2.1mm jack. ‎Double check that the pins are lining up correctly -- it's easy to mix ‎this up and you can damage your board if you plug it in backwards.‎

If you're new to header usage, check out our guide on how to solder ‎headers.‎

solder_7

Cut your Stemma connector in half and strip some shielding from ‎the yellow wire. Slip a piece of heat shrink on there. ‎

solder_8

The light strand has 3 wires: power, ground, and data. The data wire ‎is directional: solder to the IN end and not the OUT end or it won't ‎work. ‎

My lights were helpfully labeled at the factory, but not all lights from ‎all sources will be labeled, and they aren't always standardized. The ‎only way to be sure you're getting it right is to test. ‎

Alligator clips can be very helpful here -- make your connections ‎temporarily and be sure everything works before your solder.‎

lightstrand_9

Testing is a little tricky here. We can't just hook the clips to a Circuit ‎Playground Express running known good code, since these lights ‎require 12v power. So, we'll need to test with our QT Py and BFF ‎setup. ‎

Connect the red and black alligator clips to wires coming from the ‎screw terminal or 2.1mm jack on the BFF, and the data wire clip to ‎the yellow wire on the stemma. If your lights don't come on, try ‎connecting JUST the data wire to the other end of the strand.‎

Once I'd figured out which wire was which, I added some color-‎coding by soldering a red wire to the power (striped) wire on the ‎connector, a yellow wire to the middle (data) wire, and a black wire ‎to the remaining (g) wire. This way, it was easy to keep the wires ‎straight once I got them inside the box.‎

If your power supply has a 2.1mm or another jack, cut it off. Thread ‎the wires through one of the cable glands from the outside so the ‎bare wire is inside the box. ‎

Slip the 3 wires from your light strand's extra connector through the ‎other cable gland. I attached a female connector to the box, since ‎my IN end on my lights has a male connector.‎

Connect all the power wires to the BFF, using either the reconnected ‎‎2.1mm jack, or a male 2.1mm screw terminal, or the included screw ‎terminals. It doesn't matter which way you connect the wires, ‎just be sure both red wires are going to + and both black wires are ‎going to -.

box_10

Splice the third (middle) wire from your connector to the yellow wire ‎from the Stemma connector and plug it into the QT Py, then plug ‎the QT Py into the BFF.‎

All wires accounted for? Double check once more that reds are ‎going to + and blacks are going to -, then plug in your light strand ‎and your power supply to light up your strand.‎

Splice the third (middle) wire from your connector to the yellow wire ‎from the stemma connector and plug it into the QT Py, then plug the ‎QT Py into the BFF.‎

All wires accounted for? Double check once more that reds are ‎going to + and blacks are going to -, then plug in your light strand ‎and your power supply to light up your strand.‎

wires_11

Troubleshooting

If your lights don't come on or act strangely, here are some things to ‎try:‎

  1. Try connecting the data wire to the other end of the strand. The ‎data wire on these lights are directional.‎‎
  2. Be sure your screw terminal connections are tight and haven't ‎pulled out. Add some zip ties to either side of the cable gland to ‎act as strain relief.‎‎
  3. Be sure you've uploaded the code successfully, and that the ‎correct data pin is specified. ‎‎
  4. If your lights are on but the colors are unexpected, try changing ‎the color order in the code. Look for a line that shows BRG, ‎RGB, GRB, etc. and just mix the letters up and re-upload. This ‎tells the code to look for Blue, then Red, then Green (or ‎whatever order you've specified). This isn't really standardized ‎so can cause the colors to come out wrong.‎‎
  5. Flickering? Try a different power supply.‎‎
  6. One light comes on? Your power and ground wires may be ‎reversed.‎

Once it's all working, tighten the cable glands and close up the box ‎with the included screws. I added some industrial Velcro to stick my ‎box to my power supply and put zip ties on the inside and outside of ‎the cable glands to add additional strain relief.‎

strainrelief_12

Herst.-Teilenr. 4600
QT PY SAMD21 WITH STEMMA QT
Adafruit Industries LLC
Herst.-Teilenr. 5882
ADAFRUIT DC POWER BFF ADD-ON FOR
Adafruit Industries LLC
Herst.-Teilenr. 3931
CASE ABS WHITE 5.231"LX2.718"W
Adafruit Industries LLC
Herst.-Teilenr. 4399
STEMMA QWIIC JST SH CABLE 50MM
Adafruit Industries LLC
Herst.-Teilenr. 369
ADAPT TERM BL 2POS TO 2.1MM PLG
Adafruit Industries LLC
Herst.-Teilenr. 368
ADAPT TERM BL 2POS TO 2.1MM JCK
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.