Artikel und Blogs

Image of Building a Dynamometer for the Openwheel Project - Part 1 Building a Dynamometer for the Openwheel Project - Part 1

Explore a custom-built dyno for hub motors using load cells and Arduino, enabling accurate power and torque measurements.

Image of The Importance of Certification in the Selection of Connector Products The Importance of Certification in the Selection of Connector Products

Certification of products ensures operational and product safety, reliability, and compatibility.

Image of The Kitronik ARCADE Max for Makecode Arcade The Kitronik ARCADE Max for Makecode Arcade

Introducing the new ARCADE Max for Makecode Arcade from Kitronik, gamification has never been this exciting! It’s our smallest handheld gamer to date but packs the biggest screen we’ve ever had!

Image of Webinar – Driving Cost Efficiency for OEMs and Panel Builders with the ATV320 Webinar – Driving Cost Efficiency for OEMs and Panel Builders with the ATV320

This webinar introduces how the Schneider Electric Altivar™ ATV320 variable frequency drive helps address motor control challenges.

Image of Dielectric Elastomer Switches: Building Logic Gates with Soft Membranes Dielectric Elastomer Switches: Building Logic Gates with Soft Membranes

When you think of "electronics," you probably picture rigid green circuit boards, silicon chips, and soldering irons. But what if you could build a circuit entirely out of soft, stretchy rubber?

Image of How to Establish a Secure Hardware Foundation for Long-Term CRA Compliance How to Establish a Secure Hardware Foundation for Long-Term CRA Compliance Datum der Veröffentlichung: 2026-04-08

Learn how to use the NXP EdgeLock secure enclave to establish a secure hardware foundation for long-term CRA compliance.

Image of Understanding the Difference Between Latching and Non-Latching Relays Der Unterschied zwischen selbsthaltenden und nicht selbsthaltenden Relais Datum der Veröffentlichung: 2026-04-07

Relais sind eine grundlegende Komponente in elektronischen Systemen, die eine zuverlässige Steuerung von Schaltkreisen in industriellen, kommerziellen und Verbraucheranwendungen ermöglichen.

Image of Connector Testing and Its Importance to User Safety and End Use Connector Testing and Its Importance to User Safety and End Use

Connector testing, performed by accredited test facilities, is an important phase in ensuring electrical connector safety.

Image of Docker Part 1: Fixing “It Works on My Machine” Docker Part 1: Fixing “It Works on My Machine"

In this post, I want to explain what Docker is, why it helps with these problems, and give a practical understanding of how it fits into development workflows.

Image of Humanoids – What Does the Future Look Like? Humanoids – What Does the Future Look Like?

The pace of innovation is accelerating rapidly, driven by advances in AI, robotics, and computing power, with the possibilities expanding beyond simple tasks.

Image of DC/DC Converters for AI Data Centers: Tackling Space and Thermal Challenges DC/DC Converters for AI Data Centers: Tackling Space and Thermal Challenges

AI data center GPUs are pushing beyond 1 kW per device resulting in rack power densities in the megawatt scale, stressing cooling schemes past comfort zones.

Image of Webinar – Meet the LAN Squad: Defeating Ethernet Design Challenges Webinar - Treffen mit dem LAN-Squad: Herausforderungen beim Ethernet-Design meistern

Entdecken Sie, wie Lösungen von Würth Elektronik maßgeschneiderte Vorteile bieten, um die Robustheit von LAN zu erhöhen, Layout-Entscheidungen zu vereinfachen und die Gesamtsystemkosten zu reduzieren.

Image of Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope

In this blog, I will walk through a simple experiment that uses an ultrasonic sensor and oscilloscope to measure how fast sound travels through the air.

Image of Select the Right Connectors to Meet Stringent Mil/Aero Electrical and Mechanical Requirements Auswahl der richtigen Steckverbinder für die strengen elektrischen und mechanischen Mil/Aero-Anforderungen Datum der Veröffentlichung: 2026-04-01

Steckverbinder für die Luft- und Raumfahrt sowie die Verteidigungsindustrie vereinen höchste Qualität in Bezug auf Materialien, Kontakt- und Gehäusedesign, Fertigung und Prüfung, um die vorgeschriebenen Anforderungen zu erfüllen.

Image of Single-Chip Systems, MCUs for Matter-Enabled Smart Home Devices Fill Multiple Mesh Network Roles Einzelchipsysteme und MCUs für Matter-fähige intelligente Heimgeräte erfüllen mehrere Rollen in Maschennetzwerken Datum der Veröffentlichung: 2026-03-31

Energieeffiziente Komponenten mit geringer Latenz von NXP unterstützen Matter-fähige Smart-Home-Netzwerke, während Entwicklungstools Entwicklern helfen, neue Prototypen zu erstellen.

Image of Power Distribution Boards: Smart Alternative to Relays Power Distribution Boards: Smart Alternative to Relays

This blog will talk about the core concepts and the theory behind the circuit schematic and how it was approached.

Image of Harnessing AI at the Edge with iWave’s Agilex™ 5 System on Module Nutzung von KI am Netzwerkrand mit dem Systemmodul Agilex™ 5 von iWave

Da die Datenverarbeitung immer näher an den Netzwerkrand (Edge) verlagert wird, werden Plattformen benötigt, die effiziente KI-Leistung mit geringer Latenz und hoher Anpassungsfähigkeit bieten.

Image of Webinar – Seven Reasons to Move from 12 V to 48 V Today Webinar - Sieben Gründe, noch heute von 12 V auf 48 V umzusteigen

Eine Diskussion darüber, warum 48 V das vorherrschende Stromversorgungsnetz wird und wie modulare Stromversorgungslösungen den Übergang beschleunigen und vereinfachen können.

Image of Simplifying Frequency Stability for High-Speed 5G and Data Converter Designs Einfachere Frequenzstabilisierung für Highspeed-5G- und -Datenwandlerdesigns Datum der Veröffentlichung: 2026-03-25

Enfahren Sie, wie die Phasenregelkreise ADF4382 von ADI mit integrierten VCOs die Frequenzstabilität und Geschwindigkeit für Highspeed-Datenwandler und 5G-Funkdesigns verbessern.

Image of Building Quantum-Resilient Embedded Systems with iWave’s Agilex™ 5 System on Module Aufbau quantenresistenter eingebetteter Systeme mit dem Agilex™-5-SoM von iWave

iWave Global hat sich mit Xiphera zusammengetan, um quantensichere kryptographische Fähigkeiten auf iWaves Altera-basierten Agilex™-5-SoMs (System on Module) bereitzustellen.