Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 6
More enhancements include the ability to place the voltage regulators and the pre-fetch engine in low power modes. Also, two more timers have been integrated to provide additional functionality. This combined with the fact that the UART includes its own baud rate generator means there are many free resources to use. The ADC sample rate has been increased to 500 ksps providing more flexibility in signal processing. Included in the ADC enhancements is the use of a slightly different voltage reference design. The reference has more options for modifying the sensitivity of a system. For example, the internal reference can drive the ADC for 1.2 V or 2.4 V which provides the capability to maximize the dynamic range of the system.
PTM Published on: 2011-06-01