Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 16
The serial interface engine (SIE) handles all of the low level processing of the incoming packets from the host and outgoing packets from the MCU. Shown in this slide are the packets defined by the USB specification. The SIE is responsible for monitoring the data as it is received and checking the validity of the complete packet. If for some reason that packet is invalid the SIE will discard the packet and not store it in the FIFO. If the packet is valid, the SIE will pass the packet to the FIFO. This limits the firmware overhead required to service the USB data transfers.
PTM Published on: 2011-06-01