Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Optical Basics

The importance of optical basics is shown here. In this diagram, the customer can see where the plant can absorb light and where LEDs emit light. The plant absorbs light at 450 nm, exactly where the 450 nm blue LED emits light. In the same way, the red LEDs emit light at 660 nm as well. One major advantage of LED technology is that monochromatic LEDs emit light where the plant can absorb it.

PTM Veröffentlicht am: