Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Thermistor Application Slide 2
Littelfuse NTC thermistors are available in various surface mount, leaded and probe mounted configurations with resistance values ranging from 100 Ohms to more than 1 megaohm at 25°C. Because of their low cost, very predictable electrical characteristics and their excellent long term stability, thermistors are generally accepted to be the “SENSOR OF CHOICE” for numerous applications including temperature measurement and control.
PTM Veröffentlicht am: