Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
UPS Systems Slide 16

On-Line UPS systems can be safely maintained while still providing continuous power to connected equipment. However, most Line-Interactive UPS systems cannot. The difference is in the On-Line UPS's power bypass feature. If an On-Line UPS experiences an internal fault or overload, it will automatically "bypass" its internal components and deliver power directly to connected equipment. In addition, On-Line UPS systems feature an external bypass switch that allows users to perform the same function manually. While select Tripp Lite Line-Interactive UPS systems are being introduced which feature an automatic internal bypass function, none feature a manual external bypass switch.

PTM Veröffentlicht am: