Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
VL6180X FlightSense Slide 9

The VL6180X is a very low power device. The graph illustrates the power consumption of the VL6180X running at ten ranging measurements per second. The convergence time is longer with darker reflectance materials, this means the convergence time is longer, and more power is needed. The power consumption of a 3 % reflectance is below 4 mA while a 17% reflectance target, which is closer to skin or most targets, is below 2 mA. This is a very power-friendly device.

PTM Veröffentlicht am: