Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
RF IPDs Overview Slide 18

For a large inductor value of 17 nH (which translates to worst case Q-factor) the Q-factor is approximately fifty at the frequency of interest (1-2 GHz). With lower inductor values, 2 – 10 nH, Q-factors can reach up to one hundred in the 1-2 GHz frequency range. The choice of substrate significantly affects Q-factor. Since ST’s IPD devices are built on non-conductive glass substrate, Q-factor and nonlinearity performances are much better compared to LTCC/ceramic devices.

PTM Veröffentlicht am: