molex"
mm a: Tarmmal
f’\ .
molox
Ratchet Hand Crimp Tool
Engarzadora Manual de Trinquete
64016-0041
Crimps
10-22 AWG
Heat Shrink
Terminals
and Splices
64016-0041
Crimps
10-22 AWG
Heat Shrink
Terminals
and Splices
ServiceGrade
™
Instructions for Crimping Terminals
Step 1: Make sure work area is clean and dry and
wear approved eye protection.
Step 2:Open tool by squeezing handles together.
Ratchet release lever will allow handles to springopen.
Select appropriate Molexterminal and verify that wire
gauge and strip lengthare within specifications.
Strip wire to specified length.Insert terminal into
correct crimp profile,then squeeze tool slightly to
hold terminal.
Step 3a(Terminals only):Place stripped wire into
terminal, makingsure it sits parallel inside terminal.
Hold wire steady in place withone hand,ensuringwire
remains seated in terminal until
fully crimped.
Step 3b(Splices only):Place stripped wire into
splice, makingsure it sits parallel and wire brush
touches tabinside splice. Hold wire steady in place
withone hand,ensuringwire remains seated in
splice until fully crimped.
Step 4:Gently squeeze tool until ratchet releases and
carefully remove crimped terminal and wire.
Step 5(Splices only): Usinguncrimped side ofsplice,
repeat Steps 3band 4.
Note:If tool ever becomes stuck or jammed in partially
closed position,DONOTforce handles open or closed.
Pushratchet release lever and
tool will open easily.
Cautions: Manual hand tools are intended for low-volumefield
repairs and should only be used for the terminals and wire gauges
specified. Tool is NOTintended for high-volume production,and
constant,repetitive use can cause hand injury. Do not work on live
circuits -tool handles are not insulated and do not protect against
electrical shock.
Restrictions: Termination crimpquality is dependent on the
conductor profile choice and skill ofthe operator. Customers
should independently verify that intended termination meets
quality and performance needs. Not all terminal,wire and profile
combinations will provide minimumpull force requirements,or
provide an acceptable crimpform.Molex makes no warranties,
express or implied,regardingthe performance or reliability ofthe
crimp,or the appropriateness ofthe tool application. Molexdoes
not certify or repair hand tools.
Visit www.molex.com/product/apptool/and download the Molex
Quality CrimpingHandbook for additional information on crimping
and pull force testing.
Instrucciones para el engarzadode terminales
Paso 1: Cerciórese que el área de trabajo estélimpia
yseca,y use la protección ocular aprobada.
Paso 2:Comprima los mangos para abrir la
herramienta. La palanca de liberación del trinquete
permitiráque se abran los mangos accionados por
resorte. Seleccione el terminal Molexapropiado y
verifique que el calibre del alambre y la longitud de
desforrado cumplan las especificaciones. Pele la
longitud de alambre especificada. Introduzca el
terminal en el perfil correcto de engarzado,
después apriete levemente la herramienta para
sujetar el terminal.
Paso 3a(Sólo para terminales):Coloque el alambre
desforrado en el terminal,cerciórese que éste asiente
paralelamente en el interior del terminal. Con una
mano,sujete firmemente el alambre en posición,
cerciórese que permanezca asentado en el terminal
hasta que quede completamente engarzado.
Paso 3b(Sólo para empalmes a tope):Coloque el
alambre desforrado en el empalme,cerciórese que se
asiente paralelamente y que la escobilla del alambre
haga contacto con la lengüeta en el interior del
empalme. Con una mano,sujete firmemente el
alambre en posición,cerciórese que permanezca
asentado en el terminal hasta que quede
completamente engarzado.
Paso 4:Apriete levemente la herramienta hasta que
se desenganche el trinquete y retire cuidadosamente
el terminal y el alambre asíengarzados.
Paso 5(Sólo para empalmes a tope):Con el lado no
engarzado del empalme,repita los Pasos 3by4.
Nota:Si la herramienta se atora o agarrota en posición
parcialmente cerrada,NO fuerce los mangos para abrir
ocerrar la herramienta. Empuje la palanca de liberación
del trinquete y la herramienta se abrirácon facilidad.
Aviso precautorio: Las herramientas manuales están destinadas
para el uso en reparaciones de campo de bajo volumen y sólo
deberán utilizarse para los calibres de terminales y alambres
especificados. Laherramienta NOestádestinada para
producciones de alto volumen y el uso constante y repetitivo
puede causar lesiones en las manos. No trabaje en circuitos
energizados,los mangos de la herramienta no tienen aislamiento
y no le protegerán contra descargas eléctricas.
Restricciones: La calidad del engarzado de la terminación
depende de la elección de perfil del conductor y de la aptitud del
operario. Los clientes deben verificar independientemente que las
terminaciones obtenidas cumplan con las necesidades de calidad y
desempeño. No todas las combinaciones de terminales,alambres y
perfiles proporcionarán los requisitos mínimos de fuerza de tiro ni
proporcionarán una forma aceptable de engarzado.
Molexno
ofrece ninguna garantía,expresa o implícita,respecto al
desempeño o a la fiabilidad del engarzado,ni a la idoneidad de la
aplicación de la herramienta. Molexno certifica ni repara
herramientas manuales.
Visite www.molex.com/product/a[[tool/y descargue el Manual de
Engarzado de Calidad Molexpara obtener información adicional
sobre el engarzado y las pruebas de fuerza de tiro.
64016-004164016-0041
Ratchet Hand
Crimp Tool
Engarzadora Manual
de Trinquete
Molex ServiceGrade Ratchet Hand
Crimp Tool is the tool of choice for
electrical contractors, technicians and
repairmen. The sturdy construction and
comfortable, anti-slip handle grips make
ServiceGrade Ratchet Hand Crimp Tool the
perfect companion for low-volume field
repairs.
Crimps heat shrink terminals and
splices 10-22 AWG (rings, spades,
hooks, 3 and 4 ways)
Full cycling ensures complete crimps
Small handle spread - ideal for all users
Crimp release for operator safety
La Engarzadora Manual de Trinquete
Molex ServiceGrade es la herramienta
preferida de los contratistas eléctricos,
técnicos y expertos en reparación. Las
cómodas empuñaduras de los mangos de
construcción robusta y antideslizante
convierten a la Engarzadora Manual de
Trinquete ServiceGrade en el complemento
perfecto para reparaciones de campo de
bajo volumen.
Para el engarzado de terminales y
empalmes termoencogibles 10-22 AWG
(anillos, bayonetas, ganchos, de 3 y 4 vías)
El ciclo total permite obtener engarzados
completos
La poca separación de los mangos es
ideal para todos los usuarios
Con liberación de engarzado para
seguridad del operador
Made in Taiwan Hecho en Taiwán
Terminal Type
Tipo de Terminal
Terminals
Terminales
(Rings,spades, hooks,
block spades, flanged spades)
(Anillos, bayonetas, ganchos,
bayonetas de bloque,
bayonetas con reborde)
Splices
Empalmes
(Butt splices or parallel splices)
(Empalmes a tope o paralelos)
AWG Pull Force Min.-N(lb)
AWG Fuerza de Tiro Mínima -N(lb)
10 178.0(40.00)
12 155.7(35.00)
14111.2(25.00)
16 66.8(15.00)
18 44.5(10.00)
20 44.5(10.00)
22 35.6(8.00)
10 356.0(80.00)
12 311.5(70.00)
14222.6(50.00)
16 133.5(30.00)
18 89.0(20.00)
20 57.9(13.00)
22 35.6(8.00)
Molex, Incorporated
2222 Wellington Court
Lisle, Illinois 60532 U.S.A.
Tel: 630-969-4550
Fax: 630-969-1352
www.molex.com 0502
ServiceGrade
™
-Function Tool
Hmienta Para Uso Múltiple
rviceGrade
™
0039
C trips
aimps
AWG
ed and
Ulated
Tal,
s
D’s
60039
C trips
aimps
AWG
ed and
Ulated
Tal,
s
D’s
64016-003964016-0039
Make sure work area is clean and dry and wear
approved eye protection.
Instructions for Stripping Wires:
Select proper wire gauge and strip length for
application. Open handles, place wire in proper
stripping hole with the desired strip length, squeeze
handles, and pull insulation off of end of wire.
Instructions for Cutting Wires:
Select proper wire gauge, open handles, place on
cutting blade and squeeze handles until wire is cut.
Instructions for Cutting Screws and Bolts:
Select proper bolt or screw, open handles, thread into
proper hole to desired cut length (add .125" for tool
thickness),and squeeze handles to snap bolt or screw.
Instructions for Crimping:
Select appropriate Molexterminal and verifythat
wire gauge and strip length are within
specifications. Strip wire to specified length. Place
terminal on open jaws of tool in correct die. Squeeze
tool slightlyto hold terminal or connector. Place
stripped wire into terminal, making sure it sits
parallel inside terminal and wire brush is fully
inserted. Hold wire steadyin place with one hand,
ensuring wire remains seated in terminal until fully
crimped. Gentlysqueeze tool until fullycrimped.
Cautions: Manual hand tools are intended for low-volume
field repairs and should onlybe used for the terminals and
wire gauges specified. Tool is NOTintended for high-volume
production, and constant, repetitive use can cause hand injury.
Do not workon live circuits -tool handles are not insulated
and do not protect against electrical shock.
Restrictions: Termination crimp qualityis dependent on the
conductor profile choice and skill of the operator. Customers
should independently verifythat intended termination meets
qualityand performance needs. Not all terminal, wire and
profile combinations will provide minimumpull force
requirements, or provide an acceptable crimp
form.Molex makes no warranties, express or implied,
regarding the performance or reliabilityof the crimp, or the
appropriateness of the tool application. Molexdoes not certify
or repair hand tools.
Visit www.molex.com/product/apptool/and download the
MolexQualityCrimping Handbookfor additional information
on crimping and pull force testing.
Cerciórese que el área de trabajo estélimpia y
seca,y use la protección ocular aprobada.
Instrucciones para Pelar Alambres:
Seleccione el calibre de alambre yla longitud de
desforrado apropiados para la aplicación. Abra los
mangos de la herramienta, coloque el alambre en el
orificio de desforrado apropiado con la longitud de
desforrado deseada, apriete los mangos de la
herramienta yhale el aislamiento para pelar el
extremo del alambre.
Instrucciones para Cortar Alambres:
Seleccione el calibre de alambre apropiado, abra los
mangos de la herramienta, colóquelo sobre la
cuchilla de corte yapriete los mangos de la
herramienta hasta cortar completamente el
alambre.
Instrucciones para Cortar Tornillos y Pernos:
Seleccione el perno o tornillo apropiado, abra los
mangos de la herramienta, enrósquelo en el orificio
apropiado hasta lograr la longitud de corte deseada
(añada 0.125" [ 3 mm]para compensar el grosor
de la herramienta),yapriete los mangos de la
herramienta hasta cortar el perno o tornillo.
Instrucciones para el Engarzado:
Seleccione el terminal Molexapropiado y verifique
que el calibre del alambre yla longitud de
desforrado cumplan las especificaciones. Pele la
longitud de alambre especificada. Coloque el
terminal en las quijadas abiertas de la herramienta y
en el dado apropiado. Apriete levemente la
herramienta para sujetar el terminal o el conector.
Coloque el alambre desforrado en el terminal, y
asegúrese que éste asiente en posición paralela
dentro del terminal yque la escobilla del alambre
estécompletamente insertada. Con una mano,
sujete firmemente el alambre en posición,
cerciórese que permanezca asentado en el terminal
hasta que quede completamente engarzado. Apriete
suavemente la herramienta hasta lograr el
engarzado completo.
Aviso Precautorio: Las herramientas manuales están
destinadas para el uso en reparaciones de campo de bajo
volumen ysólo deberán utilizarse para los calibres de
terminales yalambre especificados. La herramienta NO está
destinada para producciones de alto volumen yel uso
constante yrepetitivo puede causar lesiones en las manos.
No trabaje en circuitos energizados, los mangos de la
herramienta no tienen aislamiento yno le protegerán contra
descargas eléctricas.
Restricciones: La calidad del engarzado de la terminación
depende de la elección de perfil del conductor yde la aptitud
del operario. Los clientes deben verificar independientemente
que las terminaciones obtenidas cumplan con las
necesidades de calidad ydesempeño. No todas las
combinaciones de terminales, alambres yperfiles
proporcionarán los requisitos mínimos de fuerza de tiro ni
proporcionarán una forma aceptable de engarzado. Molexno
ofrece ninguna garantía, expresa o implícita, respecto al
desempeño o a la fiabilidad del engarzado, ni a la idoneidad
de la aplicación de la herramienta. Molexno certifica ni
repara herramientas manuales.
Visite www.molex.com/product/apptool/ydescargue el
Manual de Engarzado de Calidad Molexpara obtener
información adicional sobre el engarzado ylas pruebas de
fuerza de tiro.
Multi-Function Tool
Herramienta Para Uso Múltiple
Molex ServiceGrade Multi-Function
Wire Tool is the tool of choice for
electrical contractors, technicians and
repairmen. It cuts screws, bolts, strips and
measures wire, and crimps terminals. The
sturdy construction and comfortable,
anti-slip handle grips make ServiceGrade
Multi-Function Wire Tool the perfect
companion for low-volume field repairs.
Cutsavariety of screw sizes (8-32,
1
0-24, 10-32, 6-32, 4-40)
Strips 10-22 AWG wire
Crimps 10-22 AWG, insulated and
non-insulated terminals
Knife blade easily cuts wires
Stripping holes can be used to
measure wire gauge
Small handle spread - ideal for
allusers
Compact and portable, only 9" long
LaHerramienta Para Uso Múltiple Molex
ServiceGrade Para Alambre
es la
herramienta preferida de los contratistas
eléctricos, técnicos y expertos en
reparación. Corta tornillo, pernos, desforra y
mide alambre, además engarza terminales.
La construcción robusta y las cómodas y
antideslizantes empuñaduras de los
mangos convierten a la Herramienta Para
Uso Múltiple ServiceGrade Para Alambre es
la herramienta ideal para reparaciones de
bajo volumen en el campo.
Corta una diversidad de tamaños de
tornillo (8-32, 10-24, 10-32, 6-32, 4-40)
Desforra alambre 10-22 AWG
Engarza terminales 10-22 AWG, con
aislamiento y sin aislamiento
La cuchilla corta alambres con facilidad
Los orificios para desforrado se pueden
utilizar para medir el calibre del alambre
La poca separación de los mangos es
ideal para todos los usuarios
Compacta y portátil, con sólo 9"
de longitud
Made in Taiwan Hecho en Taiwán
+
–
ServiceGrade
™
Molex, Incorporated
2222 Wellington Court
Lisle, Illinois 60532 U.S.A.
Tel: 630-969-4550
Fax: 630-969-1352
www.molex.com 0502
Multi-Function Tool
Herramienta Para Uso Múltiple
ServiceGrade
™
64016-0039
Cuts, Strips
and Crimps
10-22 AWG
Insulated and
Uninsulated
Terminal,
Splices
and QD’s
64016-0039
Cuts, Strips
and Crimps
10-22 AWG
Insulated and
Uninsulated
Terminal,
Splices
and QD’s
64016-003964016-0039
Make sure work area is clean and dry and wear
approved eye protection.
Instructions for Stripping Wires:
Select proper wire gauge and strip length for
application. Open handles, place wire in proper
stripping hole with the desired strip length, squeeze
handles, and pull insulation off of end of wire.
Instructions for Cutting Wires:
Select proper wire gauge, open handles, place on
cutting blade and squeeze handles until wire is cut.
Instructions for Cutting Screws and Bolts:
Select proper bolt or screw, open handles, thread into
proper hole to desired cut length (add .125" for tool
thickness), and squeeze handles to snap bolt or screw.
Instructions for Crimping:
Select appropriate Molex terminal and verify that
wire gauge and strip length are within
specifications. Strip wire to specified length. Place
terminal on open jaws of tool in correct die. Squeeze
tool slightly to hold terminal or connector. Place
stripped wire into terminal, making sure it sits
parallel inside terminal and wire brush is fully
inserted. Hold wire steady in place with one hand,
ensuring wire remains seated in terminal until fully
crimped. Gently squeeze tool until fully crimped.
Cautions: Manual hand tools are intended for low-volume
field repairs and should only be used for the terminals and
wire gauges specified. Tool is NOT intended for high-volume
production, and constant, repetitive use can cause hand injury.
Do not work on live circuits - tool handles are not insulated
and do not protect against electrical shock.
Restrictions: Termination crimp quality is dependent on the
conductor profile choice and skill of the operator. Customers
should independently verify that intended termination meets
quality and performance needs. Not all terminal, wire and
profile combinations will provide minimum pull force
requirements, or provide an acceptable crimp
form. Molex makes no warranties, express or implied,
regarding the performance or reliability of the crimp, or the
appropriateness of the tool application. Molex does not certify
or repair hand tools.
Visit www.molex.com/product/apptool/ and download the
Molex Quality Crimping Handbook for additional information
on crimping and pull force testing.
Cerciórese que el área de trabajo esté limpia y
seca, y use la protección ocular aprobada.
Instrucciones para Pelar Alambres:
Seleccione el calibre de alambre y la longitud de
desforrado apropiados para la aplicación. Abra los
mangos de la herramienta, coloque el alambre en el
orificio de desforrado apropiado con la longitud de
desforrado deseada, apriete los mangos de la
herramienta y hale el aislamiento para pelar el
extremo del alambre.
Instrucciones para Cortar Alambres:
Seleccione el calibre de alambre apropiado, abra los
mangos de la herramienta, colóquelo sobre la
cuchilla de corte y apriete los mangos de la
herramienta hasta cortar completamente el
alambre.
Instrucciones para Cortar Tornillos y Pernos:
Seleccione el perno o tornillo apropiado, abra los
mangos de la herramienta, enrósquelo en el orificio
apropiado hasta lograr la longitud de corte deseada
(añada 0.125" [ 3 mm] para compensar el grosor
de la herramienta), y apriete los mangos de la
herramienta hasta cortar el perno o tornillo.
Instrucciones para el Engarzado:
Seleccione el terminal Molex apropiado y verifique
que el calibre del alambre y la longitud de
desforrado cumplan las especificaciones. Pele la
longitud de alambre especificada. Coloque el
terminal en las quijadas abiertas de la herramienta y
en el dado apropiado. Apriete levemente la
herramienta para sujetar el terminal o el conector.
Coloque el alambre desforrado en el terminal, y
asegúrese que éste asiente en posición paralela
dentro del terminal y que la escobilla del alambre
esté completamente insertada. Con una mano,
sujete firmemente el alambre en posición,
cerciórese que permanezca asentado en el terminal
hasta que quede completamente engarzado. Apriete
suavemente la herramienta hasta lograr el
engarzado completo.
Aviso Precautorio: Las herramientas manuales están
destinadas para el uso en reparaciones de campo de bajo
volumen y sólo deberán utilizarse para los calibres de
terminales y alambre especificados. La herramienta NO está
destinada para producciones de alto volumen y el uso
constante y repetitivo puede causar lesiones en las manos.
No trabaje en circuitos energizados, los mangos de la
herramienta no tienen aislamiento y no le protegerán contra
descargas eléctricas.
Restricciones: La calidad del engarzado de la terminación
depende de la elección de perfil del conductor y de la aptitud
del operario. Los clientes deben verificar independientemente
que las terminaciones obtenidas cumplan con las
necesidades de calidad y desempeño. No todas las
combinaciones de terminales, alambres y perfiles
proporcionarán los requisitos mínimos de fuerza de tiro ni
proporcionarán una forma aceptable de engarzado. Molex no
ofrece ninguna garantía, expresa o implícita, respecto al
desempeño o a la fiabilidad del engarzado, ni a la idoneidad
de la aplicación de la herramienta. Molex no certifica ni
repara herramientas manuales.
Visite www.molex.com/product/apptool/ y descargue el
Manual de Engarzado de Calidad Molex para obtener
información adicional sobre el engarzado y las pruebas de
fuerza de tiro.
Multi-Function Tool
Herramienta Para Uso Múltiple
Molex ServiceGrade Multi-Function
Wire Tool is the tool of choice for
electrical contractors, technicians and
repairmen. It cuts screws, bolts, strips and
measures wire, and crimps terminals. The
sturdy construction and comfortable,
anti-slip handle grips make ServiceGrade
Multi-Function Wire Tool the perfect
companion for low-volume field repairs.
Cuts a variety of screw sizes (8-32,
10-24, 10-32, 6-32, 4-40)
Strips 10-22 AWG wire
Crimps 10-22 AWG, insulated and
non-insulated terminals
Knife blade easily cuts wires
Stripping holes can be used to
measure wire gauge
Small handle spread - ideal for
all users
Compact and portable, only 9" long
La Herramienta Para Uso Múltiple Molex
ServiceGrade Para Alambre
es la
herramienta preferida de los contratistas
eléctricos, técnicos y expertos en
reparación. Corta tornillo, pernos, desforra y
mide alambre, además engarza terminales.
La construcción robusta y las cómodas y
antideslizantes empuñaduras de los
mangos convierten a la Herramienta Para
Uso Múltiple ServiceGrade Para Alambre es
la herramienta ideal para reparaciones de
bajo volumen en el campo.
Corta una diversidad de tamaños de
tornillo (8-32, 10-24, 10-32, 6-32, 4-40)
Desforra alambre 10-22 AWG
Engarza terminales 10-22 AWG, con
aislamiento y sin aislamiento
La cuchilla corta alambres con facilidad
Los orificios para desforrado se pueden
utilizar para medir el calibre del alambre
La poca separación de los mangos es
ideal para todos los usuarios
Compacta y portátil, con sólo 9"
de longitud
Made in Taiwan Hecho en Taiwán
+
–
ServiceGrade
™
Molex, Incorporated
2222 Wellington Court
Lisle, Illinois 60532 U.S.A.
Tel: 630-969-4550
Fax: 630-969-1352
www.molex.com 0502
Multi-Function Tool
Herramienta Para Uso Múltiple
ServiceGrade
™
64016-0039
Cuts, Strips
and Crimps
10-22 AWG
Insulated and
Uninsulated
Terminal,
Splices
and QD’s
64016-0039
Cuts, Strips
and Crimps
10-22 AWG
Insulated and
Uninsulated
Terminal,
Splices
and QD’s
64016-003964016-0039
Make sure work area is clean and dry and wear
approved eye protection.
Instructions for Stripping Wires:
Select proper wire gauge and strip length for
application. Open handles, place wire in proper
stripping hole with the desired strip length, squeeze
handles, and pull insulation off of end of wire.
Instructions for Cutting Wires:
Select proper wire gauge, open handles, place on
cutting blade and squeeze handles until wire is cut.
Instructions for Cutting Screws and Bolts:
Select proper bolt or screw, open handles, thread into
proper hole to desired cut length (add .125" for tool
thickness), and squeeze handles to snap bolt or screw.
Instructions for Crimping:
Select appropriate Molex terminal and verify that
wire gauge and strip length are within
specifications. Strip wire to specified length. Place
terminal on open jaws of tool in correct die. Squeeze
tool slightly to hold terminal or connector. Place
stripped wire into terminal, making sure it sits
parallel inside terminal and wire brush is fully
inserted. Hold wire steady in place with one hand,
ensuring wire remains seated in terminal until fully
crimped. Gently squeeze tool until fully crimped.
Cautions: Manual hand tools are intended for low-volume
field repairs and should only be used for the terminals and
wire gauges specified. Tool is NOT intended for high-volume
production, and constant, repetitive use can cause hand injury.
Do not work on live circuits - tool handles are not insulated
and do not protect against electrical shock.
Restrictions: Termination crimp quality is dependent on the
conductor profile choice and skill of the operator. Customers
should independently verify that intended termination meets
quality and performance needs. Not all terminal, wire and
profile combinations will provide minimum pull force
requirements, or provide an acceptable crimp
form. Molex makes no warranties, express or implied,
regarding the performance or reliability of the crimp, or the
appropriateness of the tool application. Molex does not certify
or repair hand tools.
Visit www.molex.com/product/apptool/ and download the
Molex Quality Crimping Handbook for additional information
on crimping and pull force testing.
Cerciórese que el área de trabajo esté limpia y
seca, y use la protección ocular aprobada.
Instrucciones para Pelar Alambres:
Seleccione el calibre de alambre y la longitud de
desforrado apropiados para la aplicación. Abra los
mangos de la herramienta, coloque el alambre en el
orificio de desforrado apropiado con la longitud de
desforrado deseada, apriete los mangos de la
herramienta y hale el aislamiento para pelar el
extremo del alambre.
Instrucciones para Cortar Alambres:
Seleccione el calibre de alambre apropiado, abra los
mangos de la herramienta, colóquelo sobre la
cuchilla de corte y apriete los mangos de la
herramienta hasta cortar completamente el
alambre.
Instrucciones para Cortar Tornillos y Pernos:
Seleccione el perno o tornillo apropiado, abra los
mangos de la herramienta, enrósquelo en el orificio
apropiado hasta lograr la longitud de corte deseada
(añada 0.125" [ 3 mm] para compensar el grosor
de la herramienta), y apriete los mangos de la
herramienta hasta cortar el perno o tornillo.
Instrucciones para el Engarzado:
Seleccione el terminal Molex apropiado y verifique
que el calibre del alambre y la longitud de
desforrado cumplan las especificaciones. Pele la
longitud de alambre especificada. Coloque el
terminal en las quijadas abiertas de la herramienta y
en el dado apropiado. Apriete levemente la
herramienta para sujetar el terminal o el conector.
Coloque el alambre desforrado en el terminal, y
asegúrese que éste asiente en posición paralela
dentro del terminal y que la escobilla del alambre
esté completamente insertada. Con una mano,
sujete firmemente el alambre en posición,
cerciórese que permanezca asentado en el terminal
hasta que quede completamente engarzado. Apriete
suavemente la herramienta hasta lograr el
engarzado completo.
Aviso Precautorio: Las herramientas manuales están
destinadas para el uso en reparaciones de campo de bajo
volumen y sólo deberán utilizarse para los calibres de
terminales y alambre especificados. La herramienta NO está
destinada para producciones de alto volumen y el uso
constante y repetitivo puede causar lesiones en las manos.
No trabaje en circuitos energizados, los mangos de la
herramienta no tienen aislamiento y no le protegerán contra
descargas eléctricas.
Restricciones: La calidad del engarzado de la terminación
depende de la elección de perfil del conductor y de la aptitud
del operario. Los clientes deben verificar independientemente
que las terminaciones obtenidas cumplan con las
necesidades de calidad y desempeño. No todas las
combinaciones de terminales, alambres y perfiles
proporcionarán los requisitos mínimos de fuerza de tiro ni
proporcionarán una forma aceptable de engarzado. Molex no
ofrece ninguna garantía, expresa o implícita, respecto al
desempeño o a la fiabilidad del engarzado, ni a la idoneidad
de la aplicación de la herramienta. Molex no certifica ni
repara herramientas manuales.
Visite www.molex.com/product/apptool/ y descargue el
Manual de Engarzado de Calidad Molex para obtener
información adicional sobre el engarzado y las pruebas de
fuerza de tiro.
Multi-Function Tool
Herramienta Para Uso Múltiple
Molex ServiceGrade Multi-Function
Wire Tool is the tool of choice for
electrical contractors, technicians and
repairmen. It cuts screws, bolts, strips and
measures wire, and crimps terminals. The
sturdy construction and comfortable,
anti-slip handle grips make ServiceGrade
Multi-Function Wire Tool the perfect
companion for low-volume field repairs.
Cuts a variety of screw sizes (8-32,
10-24, 10-32, 6-32, 4-40)
Strips 10-22 AWG wire
Crimps 10-22 AWG, insulated and
non-insulated terminals
Knife blade easily cuts wires
Stripping holes can be used to
measure wire gauge
Small handle spread - ideal for
all users
Compact and portable, only 9" long
La Herramienta Para Uso Múltiple Molex
ServiceGrade Para Alambre
es la
herramienta preferida de los contratistas
eléctricos, técnicos y expertos en
reparación. Corta tornillo, pernos, desforra y
mide alambre, además engarza terminales.
La construcción robusta y las cómodas y
antideslizantes empuñaduras de los
mangos convierten a la Herramienta Para
Uso Múltiple ServiceGrade Para Alambre es
la herramienta ideal para reparaciones de
bajo volumen en el campo.
Corta una diversidad de tamaños de
tornillo (8-32, 10-24, 10-32, 6-32, 4-40)
Desforra alambre 10-22 AWG
Engarza terminales 10-22 AWG, con
aislamiento y sin aislamiento
La cuchilla corta alambres con facilidad
Los orificios para desforrado se pueden
utilizar para medir el calibre del alambre
La poca separación de los mangos es
ideal para todos los usuarios
Compacta y portátil, con sólo 9"
de longitud
Made in Taiwan Hecho en Taiwán
+
–
ServiceGrade
™
Molex, Incorporated
2222 Wellington Court
Lisle, Illinois 60532 U.S.A.
Tel: 630-969-4550
Fax: 630-969-1352
www.molex.com 0502
ServiceGradeTM
Ratchet Hand Crimp Tool
Engarzadora Manual de Trinquete
64016-0041
Crimps
10-22 AWG
Heat Shrink
Terminals
and Splices