; CYPRESS
III/01M
7 chip is disab
The STK11CBB mo WFflE cycies
cessary that OE isL W1
r the ‘s‘ronE time is luiliii e
and WRITE oper
fl iay_o
d from (he nomflfi
“(Lin dress sequen
and a sequence 0‘?
i the software RE atm
RECALL cycle iheiollo
sequ
peraiions is pefloert
* Read addres
or can ri_ng 2. Read add§ ><31c8 goes="" high="" “azada="" a="" fig="" 0x="" hs="" arm="" beiore="" l_he\="" le="" oi="" an="" c_e'o\="" 35%="" 6{811w="" |="" i'="" &§="" ad="" a="" uses.="" 5="" leflg="" ut="" “u"bqmhzw="" ierna="" sramioi="" e‘ifiolai'="" ‘uem="" ce.="" th="" t="" 11="" oflw="" xecuti="" enli="" com="" speciiic="" r$955="" isé="" '="" ms="" i="" store="" cy="" n="" era§9="" oi="" i="" rsi="" per!="" ed="" by="" lemenis.="" n="" a="" s="" e="" ui="" are="" di="" :3?="" eye="" quen="" re="" rom="" store="" '="" on="" 'igsimpor="" write="" @fiie="" nene,="" liésquen="" bor="" m="" mresisiorfl:="" nitiateihe="" o="" are="" uence="" is="" @rmed="">31c8>Document Number: 001-50591 Rev. *A Page 4 of 16
Device Operation
The STK11C88 is a versatile memory chip that provides
several modes of operation. The STK11C88 can operate as a
standard 32K x 8 SRAM. A 32K x 8 array of nonvolatile storage
elements shadow the SRAM. SRAM data can be copied from
nonvolatile memory or nonvolatile data can be recalled to the
SRAM.
SRAM Read
The STK11C88 performs a READ cycle whenever CE and OE
are LOW, while WE is HIGH. The address specified on pins
A0–14 determines the 32,768 data bytes accessed. When the
READ is initiated by an address transition, the outputs are
valid after a delay of tAA (READ cycle 1). If the READ is
initiated by CE or OE, the outputs are valid at tACE or at tDOE,
whichever is later (READ cycle 2). The data outputs
repeatedly respond to address changes within the tAA access
time without the need for transitions on any control input pins,
and remain valid until another address change or until CE or
OE is brought HIGH.
SRAM Write
A WRITE cycle is performed whenever CE and WE are LOW.
The address inputs must be stable prior to entering the WRITE
cycle and must remain stable until either CE or WE goes HIGH
at the end of the cycle. The data on the common I/O pins
DQ0–7 are written into the memory if it has valid tSD, before the
end of a WE controlled WRITE or before the end of an CE
controlled WRITE. Keep OE HIGH during the entire WRITE
cycle to avoid data bus contention on common I/O lines. If OE
is left LOW, internal circuitry turns off the output buffers tHZWE
after WE goes LOW.
Software STORE
Data is transferred from the SRAM to the nonvolatile memory
by a software address sequence. The STK11C88 software
STORE cycle is initiated by executing sequential CE controlled
READ cycles from six specific address locations in exact
order. During the STORE cycle, an erase of the previous
nonvolatile data is first performed, followed by a program of
the nonvolatile elements. When a STORE cycle is initiated,
input and output are disabled until the cycle is completed.
Because a sequence of READs from specific addresses is
used for STORE initiation, it is important that no other READ
or WRITE accesses intervene in the sequence. If they
intervene, the sequence is aborted and no STORE or RECALL
takes place.
To initiate the software STORE cycle, the following READ
sequence is performed:
1. Read address 0x0E38, Valid READ
2. Read address 0x31C7, Valid READ
3. Read address 0x03E0, Valid READ
4. Read address 0x3C1F, Valid READ
5. Read address 0x303F, Valid READ
6. Read address 0x0FC0, Initiate STORE cycle
The software sequence is clocked with CE controlled READs.
When the sixth address in the sequence is entered, the
STORE cycle commences and the chip is disabled. It is
important that READ cycles and not WRITE cycles are used
in the sequence. It is not necessary that OE is LOW for a valid
sequence. After the tSTORE cycle time is fulfilled, the SRAM is
again activated for READ and WRITE operation.
Software RECALL
Data is transferred from the nonvolatile memory to the SRAM
by a software address sequence. A software RECALL cycle is
initiated with a sequence of READ operations in a manner
similar to the software STORE initiation. To initiate the
RECALL cycle, the following sequence of CE controlled READ
operations is performed:
1. Read address 0x0E38, Valid READ
2. Read address 0x31C7, Valid READ
3. Read address 0x03E0, Valid READ
4. Read address 0x3C1F, Valid READ
5. Read address 0x303F, Valid READ
6. Read address 0x0C63, Initiate RECALL cycle
Internally, RECALL is a two step procedure. First, the SRAM
data is cleared, and then the nonvolatile information is trans-
ferred into the SRAM cells. After the tRECALL cycle time, the
SRAM is once again ready for READ and WRITE operations.
The RECALL operation does not alter the data in the nonvol-
atile elements. The nonvolatile data can be recalled an
unlimited number of times.
Hardware RECALL (Power Up)
During power up or after any low power condition
(VCC<VRESET), an internal RECALL request is latched. When
VCC once again exceeds the sense voltage of VSWITCH, a
RECALL cycle is automatically initiated and takes tHRECALL to
complete.
If the STK11C88 is in a WRITE state at the end of power up
RECALL, the SRAM data is corrupted. To help avoid this
situation, a 10 Kohm resistor is connected either between WE
and system VCC or between CE and system VCC.
Not recommended for new designs.
In production to support ongoing production programs only.
[+] Feedback