Datenblatt für LP2995 Eval Board Guide von Texas Instruments

l TEXAS INSTRUMENTS _T_ O VRE,:1 25v LP2995 ' C1 0 1% VDDo = 2 5V C Vang vREF \4N : 2.5V 0 _ c5 63m: AVW Vsmz { va Vrv v,,— 1 25v ‘ GND * ’
User's Guide
SNVA056BAugust 2002Revised May 2013
AN-1241 LP2995 Evaluation Board
1 Introduction
The LP2995 evaluation board is designed to provide the design engineer with a fully functional prototype
system in which to evaluate the LP2995 in both a static environment and with a complete memory system.
There are two versions of the board, while identical in functionality they differ in the package implemented,
either an SO-8 or LLP-16 LP2995 is used. This document contains information regarding the evaluation
board. For more information regarding the LP2995, see the device-specific data sheet.
2 Schematic
The following schematic was used to create the layout.
Figure 1. Schematic
Table 1. Bill Of Materials (BOM)
Name Value Description Manufacturer Model Number
U1 LP2995 DDR Linear Regulator Texas Instruments LP2995M or LP2995LQ
C1 0.1 µF 1206 Ceramic Capacitor X7R 25V Vishay Vitrammon VJ1206Y104KXXAT
C2 330 µF 6.3 V Electrolytic Radial FC Series Panasonic EEU-FC0J331S
C3 330 µF 6.3 V Electrolytic Radial FC Series Panasonic EEU-FC0J331S
C4 Not Connected
C5 68 µF 6.3 V Electrolytic Radial FC series Panasonic EEU-FC0J680
All trademarks are the property of their respective owners.
1
SNVA056BAugust 2002Revised May 2013 AN-1241 LP2995 Evaluation Board
Submit Documentation Feedback Copyright © 2002–2013, Texas Instruments Incorporated
l TEXAS INSTRUMENTS
Application
www.ti.com
3 Application
The LP2995 evaluation board can be used immediately in either a static test environment to check
functionality or in a memory termination scheme on a motherboard. In either implementation the following
steps should be taken to ensure correct operation:
1. Connect leads from the evaluation board. The board layout has been designed to allow banana jack
sockets to be directly soldered.
2. VIN should be connected to a 2.5 V power supply. This pad connects both the AVIN and PVIN pins of the
LP2995.
3. Two GND pads have been provided for ease of use. Either is sufficient for grounding of the board.
4. The VDDQ input provides the internal divide by two reference voltage. Both VREF and VTT will track this
internal voltage, nominally a 2.5V will be applied.
5. The VREFOUT pad is the output for the VREF from the LP2995 after being bypassed by a ceramic
capacitor. This can be connected either to a multimeter for confirmation or directly to the memory
controller and DIMMS.
6. The remaining two pads are for the force and sense leads of the VTT output. These should be
connected directly to the termination plane or a multimeter if interested in verification. The output will
be regulated where the VSENSE leads connect to the VTT leads permitting the connection to a
motherboard without suffering from large resistance drops.
2AN-1241 LP2995 Evaluation Board SNVA056BAugust 2002Revised May 2013
Submit Documentation Feedback
Copyright © 2002–2013, Texas Instruments Incorporated
l TEXAS INSTRUMENTS
www.ti.com
Performance
4 Performance
The following series of scope plots shows the performance of the LP2995 evaluation board when it is
subjected to various load tests. On each of the six scope plots there are two traces. The upper trace is the
VTT output voltage that has been AC coupled with a scale of 20 mV per division. The lower trace is the
output current with a scale of 500 mA per division. All the load transients begin from an initial condition of
zero current and show magnitude. Please refer to the title to determine whether the current flow is into
(sinking) or out of (sourcing) the VTT pin. The time scale for all the plots is 2mS per division.
0.5A Load Transient (Sourcing) 1A Load Transient (Sourcing)
1.5A Load Transient (Sourcing) 0.5A Load Transient (Sinking)
1A Load Transient (Sinking) 1.5A Load Transient (Sinking)
3
SNVA056BAugust 2002Revised May 2013 AN-1241 LP2995 Evaluation Board
Submit Documentation Feedback Copyright © 2002–2013, Texas Instruments Incorporated
Board Layout
www.ti.com
The LP2995 has been designed to accommodate several different capacitor options to allow the designer
to optimize the solution for the specific application. For most desktop systems large aluminum electrolytic
capacitors will be used for their low cost. However, in height limited situations such as laptops fewer high
performance capacitors might be implemented such as specialty polymers. The table below lists some of
the capacitors that can be used and a vendor that offers that product line.
Capacitor Series Vendor Vendor Phone Number
Oscon Vishay (207) 324-4140
SP Panasonic (714) 373-7857
MLCC Taiyo Yuden (800)-348-2496
Aluminum Panasonic (714) 373-7857
5 Board Layout
Figure 2. LLP Top Side
4AN-1241 LP2995 Evaluation Board SNVA056BAugust 2002Revised May 2013
Submit Documentation Feedback
Copyright © 2002–2013, Texas Instruments Incorporated
www.ti.com
Board Layout
Figure 3. LLP Bottom Side
Figure 4. SO-8 Top Side
5
SNVA056BAugust 2002Revised May 2013 AN-1241 LP2995 Evaluation Board
Submit Documentation Feedback Copyright © 2002–2013, Texas Instruments Incorporated
{L} TEXAS INSTRUMENTS
Board Layout
www.ti.com
Figure 5. SO-8 Bottom Side
6AN-1241 LP2995 Evaluation Board SNVA056BAugust 2002Revised May 2013
Submit Documentation Feedback
Copyright © 2002–2013, Texas Instruments Incorporated
l TEXAS INSTRUMENTS
www.ti.com
Board Layout
Information SO-8 Board LLP-16 Board
Board Material FR4 FR4
Size 0.9 x 1.1 inches 0.9 x 1.1 inches
Board Thickness 0.062 inch 0.062 inch
Layers 2 2
Copper Thickness 1 oz 1 oz
Plating HASL HASL
Thermal Vias 3 6
Thermal Vias Size 25 mil 10 mil
Board Thickness 0.062 inch 0.062 inch
7
SNVA056BAugust 2002Revised May 2013 AN-1241 LP2995 Evaluation Board
Submit Documentation Feedback Copyright © 2002–2013, Texas Instruments Incorporated
IMPORTANT NOTICE
Texas Instruments Incorporated and its subsidiaries (TI) reserve the right to make corrections, enhancements, improvements and other
changes to its semiconductor products and services per JESD46, latest issue, and to discontinue any product or service per JESD48, latest
issue. Buyers should obtain the latest relevant information before placing orders and should verify that such information is current and
complete. All semiconductor products (also referred to herein as “components”) are sold subject to TI’s terms and conditions of sale
supplied at the time of order acknowledgment.
TI warrants performance of its components to the specifications applicable at the time of sale, in accordance with the warranty in TI’s terms
and conditions of sale of semiconductor products. Testing and other quality control techniques are used to the extent TI deems necessary
to support this warranty. Except where mandated by applicable law, testing of all parameters of each component is not necessarily
performed.
TI assumes no liability for applications assistance or the design of Buyers’ products. Buyers are responsible for their products and
applications using TI components. To minimize the risks associated with Buyers’ products and applications, Buyers should provide
adequate design and operating safeguards.
TI does not warrant or represent that any license, either express or implied, is granted under any patent right, copyright, mask work right, or
other intellectual property right relating to any combination, machine, or process in which TI components or services are used. Information
published by TI regarding third-party products or services does not constitute a license to use such products or services or a warranty or
endorsement thereof. Use of such information may require a license from a third party under the patents or other intellectual property of the
third party, or a license from TI under the patents or other intellectual property of TI.
Reproduction of significant portions of TI information in TI data books or data sheets is permissible only if reproduction is without alteration
and is accompanied by all associated warranties, conditions, limitations, and notices. TI is not responsible or liable for such altered
documentation. Information of third parties may be subject to additional restrictions.
Resale of TI components or services with statements different from or beyond the parameters stated by TI for that component or service
voids all express and any implied warranties for the associated TI component or service and is an unfair and deceptive business practice.
TI is not responsible or liable for any such statements.
Buyer acknowledges and agrees that it is solely responsible for compliance with all legal, regulatory and safety-related requirements
concerning its products, and any use of TI components in its applications, notwithstanding any applications-related information or support
that may be provided by TI. Buyer represents and agrees that it has all the necessary expertise to create and implement safeguards which
anticipate dangerous consequences of failures, monitor failures and their consequences, lessen the likelihood of failures that might cause
harm and take appropriate remedial actions. Buyer will fully indemnify TI and its representatives against any damages arising out of the use
of any TI components in safety-critical applications.
In some cases, TI components may be promoted specifically to facilitate safety-related applications. With such components, TI’s goal is to
help enable customers to design and create their own end-product solutions that meet applicable functional safety standards and
requirements. Nonetheless, such components are subject to these terms.
No TI components are authorized for use in FDA Class III (or similar life-critical medical equipment) unless authorized officers of the parties
have executed a special agreement specifically governing such use.
Only those TI components which TI has specifically designated as military grade or “enhanced plastic” are designed and intended for use in
military/aerospace applications or environments. Buyer acknowledges and agrees that any military or aerospace use of TI components
which have not been so designated is solely at the Buyer's risk, and that Buyer is solely responsible for compliance with all legal and
regulatory requirements in connection with such use.
TI has specifically designated certain components as meeting ISO/TS16949 requirements, mainly for automotive use. In any case of use of
non-designated products, TI will not be responsible for any failure to meet ISO/TS16949.
Products Applications
Audio www.ti.com/audio Automotive and Transportation www.ti.com/automotive
Amplifiers amplifier.ti.com Communications and Telecom www.ti.com/communications
Data Converters dataconverter.ti.com Computers and Peripherals www.ti.com/computers
DLP® Products www.dlp.com Consumer Electronics www.ti.com/consumer-apps
DSP dsp.ti.com Energy and Lighting www.ti.com/energy
Clocks and Timers www.ti.com/clocks Industrial www.ti.com/industrial
Interface interface.ti.com Medical www.ti.com/medical
Logic logic.ti.com Security www.ti.com/security
Power Mgmt power.ti.com Space, Avionics and Defense www.ti.com/space-avionics-defense
Microcontrollers microcontroller.ti.com Video and Imaging www.ti.com/video
RFID www.ti-rfid.com
OMAP Applications Processors www.ti.com/omap TI E2E Community e2e.ti.com
Wireless Connectivity www.ti.com/wirelessconnectivity
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2013, Texas Instruments Incorporated