r' r' r'
Back Panel Connectors MULTITECH'Q
Power Receptacle
Mulllznnnen‘ Conduit
pagans Terminal
of mmum Bath-aw
MULTITECH©
. '\'L'::k
Quick Stan Guide Quick Stan Guide
MultiConnect® Conduit™ Multi-Tech Systems, Inc.MultiConnect® Conduit™ Multi-Tech Systems, Inc. MultiConnect® Conduit™ Multi-Tech Systems, Inc.
Quick Start GuideQuick Start GuideQuick Start Guide
Knowledge Base
http://www.multitech.com/kb.go
Support Portal
https://support.multitech.com
MultiConnect® Conduit™ Quick Start Guide
82101450L
Copyright
This publication may not be reproduced, in whole or in part, without the specific and
express prior written permission signed by an executive officer of Multi-Tech Systems,
Inc.
All rights reserved. Copyright © 2015 by Multi-Tech Systems, Inc.
Multi-Tech Systems, Inc. makes no representations or warranties, whether express,
implied or by estoppels, with respect to the content, information, material and
recommendations herein and specifically disclaims any implied warranties of
merchantability, fitness for any particular purpose and non-infringement.
Multi-Tech Systems, Inc. reserves the right to revise this publication and to make
changes from time to time in the content hereof without obligation of Multi-Tech
Systems, Inc. to notify any person or organization of such revisions or changes.
Trademarks
MultiTech, MultiConnect, and the MultiTech logo are registered trademarks of
Multi-Tech Systems, Inc. All other brand and product names are trademarks or registered
trademarks of their respective companies.
Multi-Tech Systems, Inc.
2205 Woodale Drive
Mounds View, Minnesota 55112 U.S.A.
Phone: 763-785-3500 or 800-328-9717
Fax: 763-785-9874
Support
Business Hours:
M-F, 9am to 5pm CT
Europe, Middle East, Africa:
support@multitech.co.uk
+(44) 118 959 7774
U.S., Canada, all others:
support@multitech.com
(800) 972-2439 or (763) 717-5863
MultiConnect® Conduit™
MTCDT Quick Start
www.multitech.com
Back Panel Connectors
Regulatory Information
Additional Information
Label Description
CELL, AUX
Cellular antenna inputs.
CELL - Primary
AUX - Rx Diversity/MIMO
AP1, AP2 Slots for MultiTech accessory cards.
USB DEVICE User-defined, high-speed 480 Mbps,
standard USB 2.0 Micro B connector.
E-NET
RJ-45 receptable for standard Ethernet
10/100 Base-T.
Caution: Ethernet ports and command
ports are not designed to be connected to a
public telecommunication network.
Caution: Les ports Ethernet et de
commande ne sont pas conçus
pour être raccordés à un réseau de
télécommunications public.
USB HOST High-speed, standard USB 2.0 Type A
connector. 500mA maximum current draw.
Power 9-32 Vdc power receptacle for provided
power cord.
For additional regulatory information see www.multitech.net
47 CFR Part 15 Regulation Class B Devices
This equipment has been tested and found to comply with the limits for a
Class B digital device, pursuant to part 15 of the FCC Rules. These limits are
designed to provide reasonable protection against harmful interference in
a residential installation. This equipment generates, uses, and can radiate
radio frequency energy and, if not installed and used in accordance with
the instructions, may cause harmful interference to radio communications.
However, there is no guarantee that interference will not occur in a particular
installation. If this equipment does cause harmful interference to radio or
television reception, which can be determined by turning the equipment off
and on, the user is encouraged to try to correct the interference by one or
more of the following measures:
• Reorient or relocate the receiving antenna.
• Increase the separation between the equipment and receiver.
• Connect the equipment into an outlet on a circuit different from that to
which the receiver is connected.
• Consult the dealer or an experienced radio/TV technician for help.
Warning: Changes or modifications to this unit not expressly approved
by the party responsible for compliance could void the user’s authority to
operate the equipment.
Additional information for the
MultiConnect® Conduit™ can be found
at
www.multitech.net/developer/products/conduit
You need:
•
Phillips screwdriver
•
Non-metal tweezers or similar object
•
CR1632 standard coin lithium battery
The battery is located in the Conduit housing.
To install or replace the battery:
1. Disconnect power to the Conduit, if it is connected.
2. At the front of the Conduit housing, remove the screw
that secures the nameplate to the housing and remove the
nameplate.
3. The battery holder is located at the right side of the opening
on the underside of the PC board. Use non-metal tweezers as
necessary to remove an existing battery.
4. Orient the new battery so that the positive (+) pole is facing
down. Use your fingers or non-metal tweezers to insert the
battery into the holder.
5. Reattach the MultiTech nameplate to the housing using the
screw removed in step 2.
Replacing the Battery