Datenblatt für EFB0612HHA Spec von Delta Electronics

U ,TROVICS, INC 252‘ SHAYG YING ROAD, KIIEI SAN TEI. : 8867(0)?! 3591968 TAOYIIAIY HSIEN 333, TAIWAN, RI 0. C. FAN : 8867(0)37359l991 SPECIFICATION FOR APPROVAL Huxnxxwxxxmwmm”Mum“ Customer: Description: DC FAN Customer P/N: REV: Delta Model N0; EFBO612I‘II‘IA THIS SPECIFICATIOV DEFI‘IES THE FIFCTRICAI. AVD \IECHANICAII CHARACTERISTICS OF THE DC BRIISHIIESS AXIAL FLOW FAN. THE FAY MOTOR IS WITH TWO PIIASES AVI) FOUR POIIES. 2. CHARACTERS: MAX. AIR FLOW (AT ZERO STATIC PRE AIR PRESSURE (AT ZERO AIRFLOW) ACOIISTICAL NOISE (A 0.500 (MIN, 0.540 ) M /MIN. 21.19 (MIN. 19.07) CF (MIN. (MIN. U (continued) page: 1 A00
PART NO: INSULATION STRENGTH 10 MEG OHM MIN, AT 500 VDC (BETWEEN FRAME AND (+) TERMINAL) DIELECTRIC STRENGTH 5 mA MAX, AT 500 VAC 60 Hz ONE MINUTE, (BETWEEN FRAME AND EXTERNAL COVER OPEN TYPE 70,000 HOURS CONTINUOUS OPERATIONS AT 40 °C WITH 15 ~ 65 ZRH. I LIFE EXPECTANCE ROTATION ‘ CLOCKWISE VIEW FROM NAME PLATE SIDE I OVER CIIRRENT SHUT DOWN THE CURRENT WILL SHUT DOWN WHEN LOCKING ROTOR LEAD WIRE UL 2468 ,F, AWG #23 BLACK WIRE NEGATIVE(-) RED WIRE POSITIVEH) NOTES: 1. ALL READINGS ARE MEASI‘RED AFTER STABLY WARMING LP TIIROUGII IO MINUTES 2. THE VALUES WRI’I’TEN IN I’ARENS , ( ). ARE LIMITED SI’ECI 3. ACOUSTICAL NOISE MEASURING CONDITION: DC FAN MICROPHONE 7 \ 7 7,, <2: air="" flow="" c):i:i777="" 1m="" noise="" is="" measured="" at="" rated="" voltage="" in="" free="" air="" in="" anechoic="" chamher="" with="" b="" &="" k="" sound="" le="" il="" meter="" with="" microphone="" at="" a="" distance="" of="" one="" meter="" from="" the="" fan="" intake.="" page:="" 2="" a00="">
PART NO: DELTA MODEL: EFBOGIZHHA 3, MECHANICAL: 371. DIMENSIONS SEE DIMENSIONS DRAWING 3—2. FRAME 77777777777777777777777777777777777777777777777777777777 PLASTIC UL: 94V—0 37:3. IMPELLER PLASTIC UL: OAVLO 374. BEARING SYSTEM Two BALL BEARINGS 3—5. WEIGHT 77777777777777777777777777777777777777777777777777777777777777777777 28 GRAMS I1. ENVIRONMENTAL: x1—1I OPERATING TEMPERATURE 7777777777777777777777777 —10 T0 +70 DEGREE G 4—2 STORAGE TEMPERATURE 7777777777777777777777777777 —40 TO +75 DEGREE C x1—:L OPERATING HUMIDITY 777777777777777777777777777777777777777777 5 TO 90 z RII r’1-1I STORAGE HUMIDITY 77777777777777777777777777777777777777777777777 5 TO 95 % RII :3. PROTECTION: 5-1, LOCKED ROTOR PROTECTION IMPEDANCE OF MOTOR WINDING PROTECTS MOTOR FROM FIRE IN 96 HOURS OF LOCKED ROTOR CONDITION AT THE RATED VOLTAGE. 5723 I'OLARITY I‘ROTE ‘TION BE CAPABLE OI“ WITHSTANDING II“ REVERSE CONNECTION FOR POSITIVE IND NEGATIVE LEADS 6‘ RE OZONE DEPLETING SUBSTANCES: O—II NO CONTAINING REDS, PBEOS, CECS, PBEES, PIIDI’ES AND IICECS I I’RODUC'I'ION LOCATION 771. PRODUCTS WILL BE PRODUCED IN CHINA 0R THAILAND OR TAIWAN page: 3 A00
PART NO: II. BASIC RELIABILITY REQUIREMEVI‘: 8-1I TIIERMAL LOW TEMPERATURE: —40°C CYCLING HIGH TEMPERATURE: +BO°C SOAK TIME: 30 MINUTES ’I‘RANSI'I'ION TIME < 5="" minutes="" duty="" cycles:="" :3="" 872.="" humidity="" temperature:="" +25°c="" ~="" +65“c="" exposure="" humidity:="" 90-98%="" rh="" @="" +65°c="" for="" r’l="" holrs/cycle="" power:="" non—operating="" test="" time:="" 16!]="" hours="" 8-3.="" vibration="" temperature:="" +25°c="" orientation:="" x,="" y,="" z="" power:="" non-operating="" \tiiiration="" level:="" overall="" grms:3.2="" frequency(h2)="" psd(ga2/hz)="" 10="" 0.040="" 20="" 0.100="" 40="" 0.100="" 800="" 0.002="" 1000="" 0,002="" test="" time:="" 2="" hours="" on="" each="" orientation="" 8-1.="" mechanical="" temperature:="" +20°c="" shock="" orient="" "ion:="" x,="" y,="" z="" power:="" non-operating="" ac(,="" .ration:="" 20="" g="" min.="" pulse:="" 11="" ms="" halilsine="" wave="" number="" of="" shocks:="" 5="" shocks="" for="" each="" direction="" 875‘="" life="" 'i‘i‘iivii’i‘ira'i'ure:="" max="" ,="" operating="" temi’i‘iix‘a'i'uri‘i="" power:="" operating="" duration:="" 1000="" hoiirs="" min.="" page:="" ,1="" a00="">
PART NO: Dl‘ILlA MODEL: ICFUOUIL’, MIA 5). P 1% Q ('ITRVIC: K o * ll‘jSl ('OADITION: INI’LT \‘OI" A ’l'I-TVI’I-TIZA'FI \ . III \lII)l"\ pagv: 5 OPERATION VOLTAGE 1100“ 'I‘ICW’ICH\TITRF 637,1“ A00
PART NO: DELTA \IODEL: EFBUGIIZHHA 10‘ DIMEXSION DRAWING: LABEL: Ax Ax Ax m mm m x 2, 2mm“ \ x m mm m x f m [reoeuHHAL n EFBOB‘ZHHA“ SW6” ‘56“99‘ OF: OR r50 (1M1 ‘UU’ SE‘ZMII‘D/I‘»: 50 0+0 30 355170 M2} pave: 6 A00
@um Delta will not guarantee the performance of the products if the application condition falls A written request should be submitted to Delta prior to approval if deviation from this Please exercise caution when handling fans. Damage may be caused when pressure is applied dropped to the some special designs, there is no guarantee that the products will be free from any such safety problems or failures as caused by the introduction of powder, droplets of sentative of some unique examples and viewed as the It is very important to establish the correct polarity before connecting the fan to the power be caused to the fans if connection is according to the storage temperature limits specified. Do not store fans in a high humidity environment. We highly recommend performance testing is ck Rotor Protection feature. If you impair the rotation of the impeller for the fans that do not have this function, the performance of those fans will lead It is important to consider safety when testing the fans. A suitable fan guard should be fitted to rried out at relative (ambient) temperature and F” capacitor to the fan externally when the application calls
Descriptions:
1.
Delta will not guarantee the performance of the products if the application condition falls
outside the parameters set forth in the specification.
2.
A written request should be submitted to Delta prior to approval if deviation from this
specification is required.
3.
Please exercise caution when handling fans. Damage may be caused when pressure is applied
to the impeller, if the fans are handled by the lead wires, or if the fans are hard-
dropped to the
production floor.
4. Except as pertains to s
from any such safety problems or failures as caused by the introduction of powder, droplets of
water or encroachment of insect into the hub.
5. The above-mentioned conditions are repre
sentative of some unique examples and viewed as the
first point of reference prior to all other information.
6.
It is very important to establish the correct polarity before connecting the fan to the power
source. Positive (+) and Negative (-). Damage may
be caused to the fans if connection is
with reverse polarity, as there is no foolproof method to protect against such error.
7. Delta fans are not suitable where any corrosive fluids are introduced to their environment.
8. Please ensure all fans are stored ac
cording to the storage temperature limits specified. Do not
store fans in a high humidity environment. We highly recommend performance testing is
conducted before shipping, if the fans have been stored over 6 months.
9. Not all fans are provided with the Lo
ck Rotor Protection feature. If you impair the rotation of
the impeller for the fans that do not have this function, the performance of those fans will lead
to failure.
10. Please be cautious when mounting the fan. Incorrect mounting of fans may cause exces
s
resonance, vibration and subsequent noise.
11.
It is important to consider safety when testing the fans. A suitable fan guard should be fitted to
the fan to guard against any potential for personal injury.
12. Except where specifically stated, all tests are ca
rried out at relative (ambient) temperature and
humidity conditions of 25oC, 65%. The test value is only for fan performance itself.
13. Be certain to connect an “over 4.7µ
F” capacitor to the fan externally when the application calls
for using multiple fans in parallel, to avoid any unstable power.