W,
m
CMV20000
Evaluation System Manual
© 2012 CMOSIS bvba
4.3 SOFTWARE DETAILS
4.3.1 CONTROL AREA
The 9 controls in the Control Area are:
1. STOP APPLICATION button: Click this button to stop the application from running and exit to the labview run-
time environment. Then the window can be closed. It is required to use this button to stop the program,
instead of closing the window while it is still running.
2. GRAB SEQUENCE button: Click this button to grab a single sequence of frames. The number of frames in the
sequence is set in the ‘register settings area’ of both sensor and fpga (needed for possible composing of a full
resolution image with multiple frames). When the single grab has finished, the ‘image ‘area’ will be updated.
3. GRAB CONTINUOUS button: This button has the same function as the ‘grab single’ button. The difference is
that this button has a different latching action. By clicking it once, it will be enabled. As long as it is enabled,
the software will continuously request sequences of frames and update the image area. This mode is also
called ‘video mode’. To stop the video mode, click the ‘grab continuous button’ again. This will reset the
button to its disabled state.
4. INITIALIZE button: Click this after you have loaded a config file or after some strange behavior of the
program. This will reload the fpga with the register settings in the register settings area (which are set by a
config file), reset the sensor, upload the registers to the sensor and do an LVDS training.
5. SAVE CONFIG button: By clicking this button, a configuration file can be saved. A configuration file is a
human-readable version of the sensor register map. The saved text file has the same information as the
register map that is saved using the ‘save regmap button’. The advantage of a configuration file is that it can
be reloaded into the software using the ‘load config button’. (Tip: save the configuration files with a .txt
extension).
6. LOAD CONFIG button: By clicking this button, a configuration file can be loaded into the software. When this
is done, all settings from the ‘register settings area’ are overwritten with the information from the
configuration file. The new settings are automatically transferred to FPGA and sensor (no need to click the
‘reload FPGA button’ after loading a configuration file). (Tip: it is allowed to load a configuration file while in
video mode. The new settings will reflect in the images immediately.)
7. MESSAGE: This text box contains information about what the sensor is currently doing or if an error occurs
during image grabbing, it is reported in this text box.
8. IMAGE MODE: Here you can select which output mode and remapping you want to use (16/8/4ch)
Note: On the Desktop of the evaluation PC, there is a configuration file. This file has been saved using the ‘save config
button’. You can load this configuration file into the software with the ‘load config button’. This configuration file
contains the advised values for optimal sensor operation.