INSTRUCTION MANUAL
PFE1000FA Series
TDKLambda
<Page>
2/20
CAUTION on USE
・Product individual notes are shown in the instruction manual. If there is any difference with common notes individual notes
shall have priority.
・Before using this product, be sure to read the catalog and instruction manual. There is risk of electric shock or damage to
the product or fire due to improper use.
・Input voltage, Output current, Output power, Baseplate temperature, ambient temperature and ambient humidity should be
kept within specifications, otherwise the product will be damaged, or cause electric shock or fire.
・As our product is standard industrial use product that was manufactured by purpose that is used to an general electronics
equipment etc., it is not products that to designed for High Safety uses (Uses extremely high reliability and safety are required,
if reliability and safety has not been secured, with significant dangerousness for directly life or body) is expected. Please
consider a fail safe (systems that was provided with protection circuit protective devices or systems that redundant circuit was
mounted so that was not unstable in single failure) design enough.
・The equipment has been evaluated for use in a Pollution Degree 2 environment.
・When used in environments with strong electromagnetic field, there is possibility of product damage due to malfunction.
・When used in environments where there is conductive foreign matter, dust or liquid, there is possibility of product failure or
malfunction.
・Provide countermeasure for prevention of lightning surge voltage as there is risk of damage due to abnormal voltage.
・Take care not to apply external abnormal voltage to the output. Especially, applying reverse voltage or overvoltage more
than the rated voltage to the output might cause failure, electric shock or fire.
・Do not use this product in special environment with strong electromagnetic field, corrosive gas or conductive substances and
direct sunlight, or places where product is exposed to water or rain.
・Never operate the product under overcurrent or short circuit conditions. Insulation failure, or other damages may occur.
・Protection must be provided for Service Engineers against indirect contact with the output terminals and/or to prevent tools
being dropped across them. While working on this product, the AC input power must be switched off and the input, output,
+BC, BC and R terminal voltage should be safe level.
・The application circuits and their parameters are for reference only. Be sure to verify effectiveness of these circuits and their
parameters before finalizing the circuit design.
・Excessive stress could cause damage. Therefore, please handle with care.
・Use a FastBlow external fuse to each module to ensure safe operation and compliance with the safety standards to which it
is approved. The recommended input fuse rating within the instructions is as follows: 25A, 250V fast acting fuse.
For externally mounted fuse do not use other fuses aside from our specified and recommended fuse.
・If the externally mounted fuse is blown, do not use the product even after replacing the fuse. There is risk of abnormality
inside. Be sure to request repair to our company.
・The outputs less than 28V model has possibility that hazardous voltage may occur in output terminal depending on failure
mode. The output of these products must be protected in the end use equipment to maintain SELV.
・48V output model are considered nonSELV. End equipment manufacturers must provide protection against inadvertent
contact by a service engineer.
Note
・Consider storage of the product at normal temperature and humidity avoiding direct exposure to sunlight at environment with
minimal temperature and humidity changes. Storage of product at high temperature, high humidity and environments with severe
changes in temperature and humidity might cause deterioration, and occurrence of condensation in the product.
・When disposing product, follow disposal laws of each municipality.
・If products are exported, please register the export license application etc. by the Government of Japan according to Foreign
Exchange and Foreign Trade Control Law.
・This information in this document is subject to change without prior notice. Please refer to the latest version of the data
sheet, etc., for the most upto date specifications of the product.
・No part of this document may be copied or reproduced in any form without prior written consent TDKLambda.
Note : CE MARKING
CE Marking, when applied to a product covered by this handbook, indicates compliance with the low voltage directive.