Constant current limit with auto recovery. If the output
current is >105% for more than 4 seconds the power
supply will shut down, continuous operation in overload or
short condition may result in damage to the power supply.
[1) __.-
lp:Pdmmut(A)
mzmwmmnna)
hh:mirmmm(A)
11Hmpfiewmflec)
T:Paill(:ee)
mmwwb) :xs—zawrc
cmpkmt'nefl) :Wifil4sec
Pakmmunap) :wfihwflflwmam)
Kama-rum) :mummmmmm)
My.D='[/Txlomi 535%
hls=[b1xD+!-"2x(er)]m <54” as,="" 300mm="">54”>
TDK-Lambda
DRF120 Series
INSTRUCTION MANUAL
PA618-04-01B
3. Terminal Connecting Method
Pay attention to the input wiring. If it is connected to wrong
terminal, the power supply will be damaged.
Input must be off when making connections.
Connect (Protective Earth) terminal of input
connector to ground terminal of the equipment.
The output load line and input line shall be separated
and twisted to reduce noise sensitivity.
When connecting or removing input and output wire, do
not apply stress to PCB.
4. Explanation of Functions and Precautions
4-1. Input Voltage Range
Input voltage range is single phase 85 ~ 264VAC (47~63Hz)
can withstand 300VAC surge for 5 seconds during operation.
Input voltage which is out of specification may cause unit
damage. For cases where conformance to various safety specs
(UL, CSA, EN) are required, input voltage range will be 100
~ 240VAC (50/60Hz).
4-2. Output Voltage Range
Output voltage is set to the rated value at shipment. V.ADJ
trimmer on the front panel side can be used to adjust the
output voltage within the range specified (refer to
specifications for adjustable range).
To turn the trimmer clockwise, the output voltage will be
increased. Take note when the output voltage is increased
excessively, over voltage protection (OVP) function may
trigger and output voltage will be shut down. Furthermore,
when increasing the output voltage, reduce the output current
so as not to exceed the maximum output power.
4-3. Over Voltage Protection ( OVP )
The OVP function will shut down the output. To reset the
OVP, disconnect the input voltage from the power supply for
a minute and then re-apply. Alternatively, use CNT reset
(Remote ON/OFF: OFF to ON). The OVP point is fixed and
cannot be adjusted externally.
4-4. Over Current Protection ( OCP )
Constant current limit with auto recovery. If the output
current is >105% for more than 4 seconds the power
supply will shut down, continuous operation in overload or
short condition may result in damage to the power supply.
4-5. Peak output current
The DRF120 can deliver 150% peak current for 4
seconds aiding the startup of capacitive loads and
operation of downstream circuit breakers. The operating
conditions for peak output current are as followed:
(a) Duty cycle of peak current, D <35%
(b) < rated output power and RMS current
(c) Reduce peak current according to output derating
curve for higher ambient temperature.
(d) PSU will shut down if the peak output time exceed
4 sec.
(e) Peak output current and its duration are defined as
followed:
4-6. Output Ripple & Noise
The standard specification for maximum ripple value is
measured according to measurement circuit as below. When
load lines are longer, ripple becomes larger. In this case,
electrolytic capacitor, film capacitor, etc. might be necessary
to use across the load terminal. The output ripple cannot be
measured accurately if the probe ground lead of oscilloscope
is too long.
Oscilloscope
Bandwidth : 20MHz
+
-
P.S. C1 C2
Load
1.5m 50 Cable
300mm
C1 : 47uF Electrolytic Capacitor
C2 : 0.1uF Film Capacitor
+