UM1842 Rev 2 17/36
UM1842 Hardware layout
35
6.5 On-board audio capability
The 32F411EDISCOVERY uses an audio DAC (CS43L22) to output sounds through the
audio mini-jack connector.
The 32F411EDISCOVERY controls the audio DAC through the I2C interface and processes
digital signals through an I2S connection or analog input signal.
•The sound can come independently from different inputs:
– The ST MEMS microphone (MP45DT02 or IMP34DT05): digital using PDM
protocol or analog when using the low pass filter.
– The USB connector: from external mass storage such as a USB key, USB HDD,
and so on.
– The internal memory of the STM32F411VET6.
•The sound can be output in different ways through audio DAC:
– Using the I2S protocol
– Using the microphone output directly via a low pass filter to analog input AIN4x of
the CS43L22
6.6 USB OTG supported
The STM32F411VET6 is used to drive only USB OTG full speed on this board. The USB
micro-AB connector (CN5) allows the user to connect a host or device component, such as
a USB key, mouse, and so on.
Two LEDs are dedicated to this module:
•LD7 (green LED) indicates when VBUS is active
•LD8 (red LED) indicates an overcurrent from a connected device.
6.7 E-compass MEMS (ST MEMS LSM303DLHC or LSM303AGR)
The LSM303DLHC or LSM303AGR is an ultra-compact low-power system-in-package
featuring a 3D digital linear acceleration sensor and a 3D digital magnetic sensor. It includes
a sensing element and an IC interface able to provide the measured acceleration to the
external world through an I2C serial interface.
The LSM303DLHC has dynamically user-selectable full scales of ± 2g/± 8g and is capable
of measuring the acceleration, and a magnetic field full scale from ±1.3 g to 8.1 g with an
output data rate of 100 Hz or 400 Hz.
The LSM303AGR has linear acceleration full scales of ± 2g/± 4g/± 8g/± 16g and a magnetic
field dynamic range of ±50 gauss with an output data rate of 100 kHz, 400 kHz, 1 MHz, and
3.4 MHz.
The STM32F411VET6 MCU controls this motion sensor through the I2C interface.
6.8 Gyroscope MEMS (ST MEMS L3GD20 or I3G4250D)
The L3GD20 or I3G4250D is an ultra-compact, low-power, three-axis angular rate sensor. It
includes a sensing element and an IC interface able to provide the measured angular rate to
the external world through the I2C/SPI serial interface.