austr/amicrosystems
ASEOOD
will
360), as well as the
Magnet angle value in
degree
Raw angle value and
bargranh - same vein
the angle in degr
9 mode (w battery or use powered without our) (WSleFi
e internal (on board) AS5115 or an external device is used and w
82 to the left side the LED is turned on and one can use an
ible with the A85115-AB.
ogrammer GUI software
ling the GUI on the PC
eliminary software is developed for a Microsoft Windows XP
tnet (.NET) framework version 2.0 or more must be installed
charge from the Microsoft webpage:
ntlp:i/www.microsoflcomldownloads/details.aspx?FamiIy|D=0856eacb43624b0d-8edd-aab1505e04f5&dispiaylang=en
Following Procedure is recommended before starting t
1 check on your PC if Service Pack 2 is
2 install the mentioned .NET pack
3. execute setupexe
4 Finally start the GUI using the
4.2 The Home ta
Figure 3 shows the m
demoboard na
By default the
be automatica
AS5115 Demoboard OPERATIONAL MA NUA L
Revision 1.1, 26.02.2010 Page 2 of 10
www.austriamicrosystems.com
• As standalone unit supplied by an USB port
Connect the demoboard to a PC using a USB/USB cable (included in demoboard shipment). The board is
supplied by the 5V supply of the USB port. No other connections are required.
• As input device for the AS5000 Programmer GUI software
This configuration uses the same USB hardware connection as mentioned above, but additionally the AS5000
Programmer GUI software is running. The LCD display will be turned off and the Angle/Sine/Cosine value will
be displayed on the PC screen.
3.1 Hardware Indicators
3.1.1 Graphic LCD display
The LCD display shows the real-time absolute angle position of the magnet as a digital word (0…360), as well as the
current sine and cosine value of the output voltage.
Turning the knob clockwise will increase the angle value until 359, then 0.
Figure 2: LCD display in st and alone mode (9V battery or USB power ed without GUI)
3.1.2 EXT LED
The EXT LED indicates whether the internal (on board) AS5115 or an external device is used and which values are
shown on the display. By switching S2 to the left side the LED is turned on and one can use an external AS5115 by
connecting it at P1.
The header P1 is pin compatible with the AS5115-AB.
4 AS5000 Programmer GUI software
4.1 Installing the GUI on the PC
The preliminary software is developed for a Microsoft Windows XP operating system with Service Pack 2. In addition
the dotnet (.NET) framework version 2.0 or more must be installed on the PC. This package can be downloaded free of
charge from the Microsoft webpage:
http://www.microsoft.com/downloads/details.aspx?FamilyID=0856eacb-4362-4b0d-8edd-aab15c5e04f5&displaylang=en
Following Procedure is recommended before starting the GUI:
1. check on your PC if Service Pack 2 is installed
2. install the mentioned .NET package to your computer
3. execute setup.exe
4. Finally start the GUI using the shortcut in the start menu or desktop.
4.2 The Home tab
Figure 3 shows the main window of the GUI. On the top left corner, board information as firmware (FW) version and
demoboard name declaration can be found.
By default the GUI is in the auto detection mode. Any connected austriamicrosystems demoboard and programming tool will
be automatically detected and displayed in the right top corner. The GUI is divided into three main sections HOME, TWI and
OTP.
By selecting the TWI (AS5115 bidirectional serial protocol) tab, the information of the angular position appears. See figure 4.
COS values
- calculated angle value
bargraph - same value as
the angle in degree
(1°/step)
ams AG
Technical content still valid