Introduction
VL-EPM-E2 Reference Manual 2
RoHS Compliance
The VL-EPM-E2 is RoHS-compliant.
ABOUT ROHS
In 2003, the European Union issued Directive 2002/95/EC regarding the Restriction of the use of
certain Hazardous Substances (RoHS) in electrical and electronic equipment.
The RoHS directive requires producers of electrical and electronic equipment to reduce to
acceptable levels the presence of six environmentally sensitive substances: lead, mercury,
cadmium, hexavalent chromium, and the presence of polybrominated biphenyls (PBB) and
polybrominated diphenyl ethers (PBDE) flame retardants, in certain electrical and electronic
products sold in the European Union (EU) beginning July 1, 2006.
VersaLogic Corp. is committed to supporting customers with high-quality products and services
meeting the European Union’s RoHS directive.
Warnings
ELECTROSTATIC DISCHARGE
Warning! Electrostatic discharge (ESD) can damage circuit boards, disk drives, and other
components. The circuit board must only be handled at an ESD workstation. If an
approved station is not available, some measure of protection can be provided by
wearing a grounded antistatic wrist strap. Keep all plastic away from the board, and
do not slide the board over any surface.
After removing the board from its protective wrapper, place the board on a
grounded, static-free surface, component side up. Use an antistatic foam pad if
available.
The board should also be protected inside a closed metallic antistatic envelope
during shipment or storage.
HANDLING CARE
Warning! Care must be taken when handling the board not to touch the exposed circuitry
with your fingers. Though it will not damage the circuitry, it is possible that small
amounts of oil or perspiration on the skin could have enough conductivity to cause
the contents of CMOS RAM to become corrupted through careless handling,
resulting in CMOS resetting to factory defaults.
EARTH GROUND REQUIREMENT
Warning! All mounting standoffs should be connected to earth ground (chassis ground). This
provides proper grounding for ESD and EMI purposes.