F iiiiii
NCP1593A, NCP1593B
http://onsemi.com
11
APPLICATION INFORMATION
Programming the Output Voltage
The output voltage is set using a resistive voltage divider
from the output voltage to FB pin (see Figure 27). So the
output voltage is calculated according to Eq.1.
Vout +VFB @
R1)R2
R2
(eq. 2)
Figure 27. Output divider
FB
R2
R1
Vout
Inductor Selection
The inductor is the key component in the switching
regulator. The selection of inductor involves trade−offs
among size, cost and efficiency. The inductor value is
selected according to the equation 2.
L+
Vout
f@Iripple
@ǒ1*
Vout
Vin(max)Ǔ(eq. 3)
Where Vout − the output voltage;
f − switching frequency, 1.0 MHz;
Iripple − Ripple current, usually it’s 20% − 30% of output
current;
Vin(max) − maximum input voltage.
Choose a standard value close to the calculated value to
maintain a maximum ripple current within 30% of the
maximum load current. If the ripple current exceeds this
30% limit, the next larger value should be selected.
The inductor’s RMS current rating must be greater than
the maximum load current and its saturation current should
be about 30% higher. For robust operation in fault conditions
(start−up or short circuit), the saturation current should be
high enough. To keep the efficiency high, the series
resistance (DCR) should be less than 0.1 W, and the core
material should be intended for high frequency applications.
Output Capacitor Selection
The output capacitor acts to smooth the dc output voltage
and also provides energy storage. So the major parameter
necessary to define the output capacitor is the maximum
allowed output voltage ripple of the converter. This ripple is
related to capacitance and the ESR. The minimum
capacitance required for a certain output ripple can be
calculated by Equation 4.
COUT(min) +
Iripple
8@f@Vripple
(eq. 4)
Where Vripple is the allowed output voltage ripple.
The required ESR for this amount of ripple can be
calculated by equation 5.
ESR +
Vripple
Iripple
(eq. 5)
Based on Equation 3 to choose capacitor and check its
ESR according to Equation 4. If ESR exceeds the value from
Eq.4, multiple capacitors should be used in parallel.
Ceramic capacitor can be used in most of the applications.
In addition, both surface mount tantalum and through−hole
aluminum electrolytic capacitors can be used as well.
Input Capacitor Selection
The input capacitor can be calculated by Equation 6.
Cin(min) +Iout(max) @Dmax @1
f@Vin(ripple)
(eq. 6)
Where Vin(ripple) is the required input ripple voltage.
Dmax +
Vout
Vin(min)
is the maximum duty cycle. (eq. 7)
Power Dissipation
The NCP1593 is available in a thermally enhanced
10−pin, DFN package. When the die temperature reaches
+185°C, the NCP1593 shuts down (see the
Thermal−Overload Protection section). The power
dissipated in the device is the sum of the power dissipated
from supply current (PQ), power dissipated due to switching
the internal power MOSFET (PSW), and the power
dissipated due to the RMS current through the internal
power MOSFET (PON). The total power dissipated in the
package must be limited so the junction temperature does
not exceed its absolute maximum rating of +150°C at
maximum ambient temperature. Calculate the power lost in
the NCP1593 using the following equations:
1. High side MOSFET
The conduction loss in the top switch is:
PHSON +I2RMS_HSFET RDS(on)HS (eq. 8)
Where:
IRMS_FET +ǒIout 2)
DIPP 2
12 Ǔ D
Ǹ(eq. 9)
DIPP is the peak−to−peak inductor current ripple.
The power lost due to switching the internal power high side
MOSFET is: