Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Operating System Slide 19

Shown on this slide are some size benchmarks. The ROM numbers reflect the text and constants, things that can be put in the flash on a device, whereas the RAM is data, stacks, and global data. The Static Semaphore/Task Application is an application where everything is defined by the configuration time and created via the configuration tool. The Dynamic Semaphore/Task Application has a couple of tasks more than the Semaphore, but in this case, the Task and Semaphore are created at runtime from main.

PTM Published on: 2012-09-05