Shown on this slide is a picture of the Graphical Configuration tool. This tool is opened by double clicking on the .cfg file in the project. On the left, the user can choose which modules they desire to use in this product page. The outline view is used to navigate among the modules that are being used to see the different properties and change these properties using the graphical editor in the middle pane. It is also important to note that TI supports a source view, so if the user wants to look at the raw JavaScript, they can do that with this editor pane. Finally, if the configuration script has any warnings or errors, the user will see them in the errors portion at the bottom of the window.