Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Remote Control Infrared Receivers Slide 6

Another key performance characteristic for IR receivers is transmission distance. The maximum possible transmission distance of an IR receiver is primarily a factor of the intensity of the emitter and the sensitivity of the receiver. Secondary factors include the optical reflectivity of the walls, ambient light sources (DC and AC), and the optical quality of the receiver housing window. As shown in the table, Vishay ranks #1 in transmission distance among the leading IR receiver suppliers.

PTM Published on: 2011-11-08
PTM Updated on: 2015-02-26