This slide shows the inductor current of both phases of the previous page schematic for channel 0. As can be seen, the current is well balanced between the phases even with a 10A step load. The bottom trace shows the maximum deviation from nominal due to the step-load that is less than 100mV.