*9 TEXAS
INSTRUMENTS
REFH REFL
"#$%&%%
SBOS329E − JUNE 2005 − REVISED DECEMBER 2007
www.ti.com
8
DATA RATES
The two-wire bus operates in one of three speed modes:
DStandard: allows a clock frequency of up to 100kHz;
DFast: allows a clock frequency of up to 400kHz; and
DHigh-speed mode (or Hs mode): allows a clock
frequency of up to 3.4MHz.
The BUF20800 is fully compatible with all three modes. No
special action is required to use the device in Standard or
Fast modes, but High-speed mode must be activated. To
activate High-speed mode, send a special address byte of
00001xxx, with SCL = 400kHz, following the START
condition; xxx are bits unique to the Hs-capable master,
which can be any value. This byte is called the Hs master
code. (Note that this is different from normal address
bytes—the low bit does not indicate read/write status.) The
BUF20800 will respond to the High-speed command
regardless of the value of these last three bits. The
BUF20800 will not acknowledge this byte; the
communication protocol prohibits acknowledgement of
the Hs master code. On receiving a master code, the
BUF20800 will switch on its Hs mode filters, and
communicate at up to 3.4MHz. Additional high-speed
transfers may be initiated without resending the Hs mode
byte by generating a repeat START without a STOP. The
BUF20800 will switch out of Hs mode with the next STOP
condition.
GENERAL CALL RESET AND POWER-UP
The BUF20800 responds to a General Call Reset, which
is an address byte of 00h (0000 0000) followed by a data
byte of 06h (0000 0110). The BUF20800 acknowledges
both bytes. Upon receiving a General Call Reset, the
BUF20800 performs a full internal reset, as though it had
been powered off and then on. It always acknowledges the
General Call address byte of 00h (0000 0000), but does
not acknowledge any General Call data bytes other than
06h (0000 0110).
The BUF20800 automatically performs a reset upon
power up. As part of the reset, all outputs are set to
(VREFH −V
REFL)/2. Other reset values are available as a
custom modification—contact your TI representative for
details.
The BUF20800 resets all outputs to (VREFH −V
REFL)/2
after sending the device address, if a valid DAC address
is sent with bits D7 to D5 set to ‘100’. If these bits are set
to ‘010’, only the DAC being addressed in this most
significant byte (MSB) and the following least significant
byte (LSB) will be reset.
OUTPUT VOLTAGE
Buffer output values are determined by the reference
voltages (VREFH and VREFL) and the decimal value of the
binary input code used to program that buffer. The value is
calculated using Equation 1:
VOUT +ƪVREFH *VREFL
1024 Decimal Value of Codeƫ)VREFL
The valid voltage ranges for the reference voltages are:
4V vVREFH vVS*0.2V and 0.2V vVREFL vVS*4V
The BUF20800 outputs are capable of a full-scale voltage
output change in typically 5µs—no intermediate steps are
required.
OUTPUT LATCH
Updating the DAC register is not the same as updating the
DAC output voltage, because the BUF20800 features a
double-buffered register structure. There are three
methods for latching transferred data from the storage
registers into the DACs to update the DAC output
voltages.
Method 1 requires externally setting the latch pin (LD)
LOW, LD = LOW, which will update each DAC output
voltage whenever its corresponding register is updated.
Method 2 externally sets LD = HIGH to allow all DAC
output voltages to retain their values during data transfer
and until LD = LOW, which will then simultaneously update
the output voltages of all DACs to the new register values.
Use this method to transfer a future data set in advance to
prepare for a very fast output voltage update.
Method 3 uses software control. LD is maintained HIGH,
and all DACs are updated when the master writes a 1 in bit
15 of any DAC register. The update will occur after
receiving the 16-bit data for the currently-written register.
The General Call Reset and the power-up reset will update
the DAC regardless of the state of the latch pin.
READ/WRITE OPERATIONS
The BUF20800 is able to read from a single DAC, or
multiple DACs, or write to the register of a single DAC, or
multiple DACs in a single communication transaction.
DAC addresses begin with 0000 0000, which corresponds
to DAC_1, through 0001 0011, which corresponds to
VCOM OUT2.
Write commands are performed by setting the read/write
bit LOW. Setting the read/write bit HIGH will perform a read
transaction.
(1)
(2)