CY4541 EZ-PD, CCG4 EVK Quick Start Guide Datasheet by Infineon Technologies

\ on CCG EVK base boards and CYASM CCGA daughter curd stew
CY4541 EZ-PD
TM
CCG4 EVK
QUICK START GUIDE
STEP
1
STEP
2
Unpack the kit contents
Note: Color of the solder mask used on CCG EVK base boards and CY4541 CCG4 daughter card
may vary from the image shown in step1.
Jumper Wire
USB 2.0 Type-A
to Mini-B Cable
USB 3.0 EMCA Type-C Cable
USB 3.0 Type-A
to Type-B Cables
24V DC Power Adapter
Screwdriver
USB Type-C to
Type-A Adapters
Verify that the user LED jumper (J11) is populated on CCG EVK base board 1 (connected to Port 1of
CCG4 daughter card) and that the voltage selection jumper (J5) on the CCG4 daughter card is set to
3.3 V (position 1-2). Ensure that the wires are connected with correct polarity between the power
provider header (J12) of both the CCG EVK base boards as shown in the figure in step2. Connect the
DC power adapter (provided with the kit) to the DC power jack (J1) of either of the CCG EVK base
boards.Verify that the setup is as shown in the figure in step2. Plug the other end of the DC power
adapter to the AC power socket. LED1 (Green) on the CCG4 daughter card and on both the CCG EVK
base boards glow to indicate that the kit is powered. In addition, the LED2 (Orange) on the CCG EVK
base board 1 blinks continuously to indicate that CCG4 is powered and active.
J5
J11
LED1
(on CCG4
Daughter Card)
Port 1
J12
J1
Red color wire to the
+ve terminal
LED1 (on CCG
EVK Base Board 1)
LED2 (on CCG
EVK Base Board 1)
LED1(on CCG EVK Base Board 2)
CCG
EVK Base Board 1
CCG EVK Base Board 2
CY4541 CCG4
Daughter Card J12
J1
Red color wire to the
+ve terminal
+
+
DC Power Adapter
Connected to CCG
EVK Base Board 1 Note: Ensure that CCG4 daughter
card is firmly connected to the
CCG EVK base boards.
CCG EVK
Base Board
CCG EVK
Base Board
CY4541 CCG4
Daughter Card
nnnnnnnnnnnnnnnnnnn
USB 3.0 Type-A to Type-B
cable connected to CCG
EVK Base Board 2
USB 3.0 enabled notebook or PC is recommended
USBUSB
J2
J2
J3 J3
USB 3.0 Type-A
to Type-B cable
connected to
CCG EVK
Base Board 1
CY4541 EZ-PD
TM
CCG4 EVK
QUICK START GUIDE
STEP
3
Connect each USB 3.0 Type-A to Type-B cable from the PC to the USB Type-B port (J2) of each
of the CCG EVK base boards. Connect each USB Type-C to Type-A adapter to the USB Type-C
port (J3) of each of the CCG EVK base boards. Plug USB pendrives (not provided with the kit)
into both the USB Type-C to Type-A adapters. Verify that the setup is as shown in the figure in
step3. Observe the enumeration of both the USB pendrives on the PC. Initiate data transfer between
the two USB pendrives, and observe the data transfer speed*. This step demonstrates the capability
of CCG4 to control two USB Type-C interfaces simultaneously.
STEP
4
Refer to the CY4541 Kit guide** for a detailed explanation of the Dual Role Port (DRP) and
Type-C to Display Port demo using CCG4.
** Download and install the CY4541 CCG4 EVK complete setup from www.cypress.com/CY4541
to access the kit design files and documentation. After the installation, CY4541 Kit Guide.pdf
will be available at C:\Program Files (x86)\Cypress\CY4541 CCG4 EVK\1.0\Documentation\
CY4541 Kit Guide.pdf (on 64-bit Windows operating systems)
or
C:\Program Files\Cypress\CY4541 CCG4 EVK\1.0\Documentation\CY4541 Kit Guide.pdf
(on 32-bit Windows operating systems)
Note that any USB device can be used instead of a pendrive with the setup shown in step3.
* Data transfer speed depends on the type of the USB port (SuperSpeed or High Speed) of the PC,
the pendrive (SuperSpeed or High Speed) and the system configuration.
© 2016 - 2017 Cypress Semiconductor Corporation. All rights reserved.
All trademarks or registered trademarks referenced herein are the properties of their respective owners.
002-10266 Rev.*F
USB Pen-drive
USB Pen-drive
USB Type-C to
Type-A Adapter
USB Type-C to
Type-A Adapter